cancel
Showing results for 
Search instead for 
Did you mean: 

Nor Flash

tigerdluffy
New Contributor

Hi,

Can I get thermal resistance theta j-a, theta j-b, theta j-c, and max junction temperature of S70FL01GSAGBHIC10 device?

0 Likes
1 Solution
BushraH_91
Moderator
Moderator

Hello,

Thank you for contacting Cypress Technical Support, an Infineon Technologies Company. Please see below

Theta JA = 37.4 °C/W 

Theta JB = 11.7 °C/W 

Theta JC = 10.5 °C/W

To calculate Max Junction Temperature, please specify mode and frequency

Serial SDR @ 50 MHz
Serial SDR @ 133 MHz
Quad SDR @ 80 MHz
Quad SDR @ 104 MHz
Quad DDR @ 66 MHz
Quad DDR @ 80 MHz

Thank you

Regards,

Bushra

View solution in original post

0 Likes
1 Reply
BushraH_91
Moderator
Moderator

Hello,

Thank you for contacting Cypress Technical Support, an Infineon Technologies Company. Please see below

Theta JA = 37.4 °C/W 

Theta JB = 11.7 °C/W 

Theta JC = 10.5 °C/W

To calculate Max Junction Temperature, please specify mode and frequency

Serial SDR @ 50 MHz
Serial SDR @ 133 MHz
Quad SDR @ 80 MHz
Quad SDR @ 104 MHz
Quad DDR @ 66 MHz
Quad DDR @ 80 MHz

Thank you

Regards,

Bushra

View solution in original post

0 Likes