- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
What is the procedure of restoring the memory to the factory state when SPI Status Register 1 = 0x41
This can be done through the SafeBoot recovery option.
I want to set the default value of SR / CR
Attached is part of the report from Infineon.
I would like to use the JTAG interface to fix this problem.
//
#DEFINE ERASE WD=0x06 CE_HI WD=0xDC ADDR_CYCLE4=SA ADDR_CYCLE3=SA ADDR_CYCLE2=SA ADDR_CYCLE1=SA CE_HI WD=0x05 read_status=0bX00XXXX0 CE_HI
#PROGRAM WD=0x06 CE_HI WD=0x12 ADDR_CYCLE4=PA ADDR_CYCLE3=PA ADDR_CYCLE2=PA ADDR_CYCLE1=PA PAGE_SIZE*WD=pd CE_HI WD=0x05 read_status=0bX00XXXX0 CE_HI
#DEFINE PROGRAM WD=0x06 CE_HI WD=0x12 ADDR_CYCLE4=PA ADDR_CYCLE3=PA ADDR_CYCLE2=PA ADDR_CYCLE1=PA WD=pd CE_HI WD=0x05 read_status=0bX00XXXX0 CE_HI
#DEFINE UNLOCK WD=0x06 CE_HI WD=0x01 WD=0x00 CE_HI WD=0x05 read_status=0b00000000 CE_HI
#DEFINE LOCK WD=0x06 CE_HI WD=0x01 WD=0x1C CE_HI WD=0x05 read_status=0b00011100 CE_HI
#READ_PAGE WD=0x13 ADDR_CYCLE4=PA ADDR_CYCLE3=PA ADDR_CYCLE2=PA ADDR_CYCLE1=PA PAGE_SIZE*RD=pd CE_HI
#DEFINE READ_ID WD=0x9F RD=MAN_ID RD=DEV_ID CE_HI
#MAN_ID=0x34
#DEV_ID=0x2A
#PROGRAM_TIME 340 750
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Here is the suggested flow to recover from register corruption failure:
- Pre-requisitions:
- Interface Protocol = Single SPI (1S-1S-1S)
- Address Bytes = 4 Byte Address Mode Only
- Frequency of Operation = Maximum
- Register Read Latency = 2 Clock Cycles
- Output Impedance = 45Ω
- SafeBoot recovery flow:
- Read Status Register 1, if SR1=0x61, it is flash initialization failure, hardware reset the board to fix the issue. If SR1=0x41, continue the following steps
- Clear Status Register (command 0x30)
- Write Enable (command 0x06)
- Write Any Register (command 0x71 + die1 register 4-byte address + desired register configuration value) (if multiple non-volatile registers need to be configured, repeat this step with respective register 4-byte address and desired registers values)
- Write Any Register (command 0x71 + die2 register 4-byte address + desired register configuration value) (if multiple non-volatile registers need to be configured, repeat this step with respective register 4-byte address and desired registers values)
- Change host controller interface to the same as register configurations.
Thank you
Regards,
Bushra