S25FL256SAGNFI003 Schematic question

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
NL
Level 1
Level 1
First question asked Welcome!

We are planning on using S25FL256SAGNFI003 in a new PCB design we are doing.  However, I was not able to find if the exposed pad should be connected electrically or left isolated as only a thermal pad.

Could you help identify how to electrically connect the exposed pad shown below?

(exposed pad shown):

NL_0-1637328458525.png

Thanks,

-Nate

0 Likes
1 Solution
Roy_Liu
Moderator
Moderator
Moderator
5 comments on KBA First comment on KBA 10 questions asked

 Hi Nate,

Please refer to this KBA - https://community.infineon.com/t5/Knowledge-Base-Articles/Exposed-Pad-Connection-in-WSON-Package-of-...

The exposed pad does not have any electrical significance and is not internally connected to the die. There is nothing electrically bonded to the pad on the bottom of the WSON package. Heat dissipation is also not a concern, even though the datasheet describes this as a heat sink slug. It is used to improve board-level reliability by attaching the pad to the board with solder. It can be connected to the ground or left unconnected.

 

Roy Liu

View solution in original post

0 Likes
1 Reply
Roy_Liu
Moderator
Moderator
Moderator
5 comments on KBA First comment on KBA 10 questions asked

 Hi Nate,

Please refer to this KBA - https://community.infineon.com/t5/Knowledge-Base-Articles/Exposed-Pad-Connection-in-WSON-Package-of-...

The exposed pad does not have any electrical significance and is not internally connected to the die. There is nothing electrically bonded to the pad on the bottom of the WSON package. Heat dissipation is also not a concern, even though the datasheet describes this as a heat sink slug. It is used to improve board-level reliability by attaching the pad to the board with solder. It can be connected to the ground or left unconnected.

 

Roy Liu
0 Likes