Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Nor Flash Forum Discussions

This widget could not be displayed.
Anonymous
Not applicable

Hi,

Can we get the SFDP table of S25FL128S flash?.

Thanks,

Sanjeev

0 Likes
1 Solution
This widget could not be displayed.
Anonymous
Not applicable

Hi Sanjeev,

Unfortunately we do not have part which have both VIO option and support SFDP.

Other than S25FL127S, S25FL128L also support SFDP but both do not have VIO option.

S25FL127S is a product developed mainly for small packaging by eliminating less requested functions and adjusting its performance. For applications that require the full-feature set and higher performance, such as DDR, Vio, faster program/erase timing, and so on, it is recommended that you strongly consider S25FL128S.

Also, for comparison between FL-S and FL-L you can refer below Application Note :

AN218107 - Migration from S25FL-S to S25FL-L Serial NOR Flash Memory | Cypress Semiconductor

Hope this help.

Thanks,

Nada

View solution in original post

0 Likes
3 Replies
This widget could not be displayed.
Anonymous
Not applicable

Hi,

Only S25FL127S and S25FL512S devices from S25FL-S family support Read Serial Flash Discoverable Parameters (RSFDP).

It is not supported in other S25FL-S devices.

You can refer to one of our Application Note from this link below:

AN98486 - Programmer’s Guide for Cypress 65-nm FL-S MirrorBit® Flash Family | Cypress Semiconductor

Thanks,

Nada

This widget could not be displayed.
Anonymous
Not applicable

Hi Nada,

Thanks for the quick reply.

Can you suggest one part which has similar electrical specification specially VIO range of 1.65V to 3.6V with SFDP option available. Size 128Mb.

Thanks,

Sanjeev

0 Likes
This widget could not be displayed.
Anonymous
Not applicable

Hi Sanjeev,

Unfortunately we do not have part which have both VIO option and support SFDP.

Other than S25FL127S, S25FL128L also support SFDP but both do not have VIO option.

S25FL127S is a product developed mainly for small packaging by eliminating less requested functions and adjusting its performance. For applications that require the full-feature set and higher performance, such as DDR, Vio, faster program/erase timing, and so on, it is recommended that you strongly consider S25FL128S.

Also, for comparison between FL-S and FL-L you can refer below Application Note :

AN218107 - Migration from S25FL-S to S25FL-L Serial NOR Flash Memory | Cypress Semiconductor

Hope this help.

Thanks,

Nada

0 Likes
This widget could not be displayed.