Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

lock attach
Attachments are accessible only for community members.
user_4140881
Level 1
Level 1

I always successfully used the S25FL064P in our design with Xilinx Spartan 6. Now the S25FL064P is obsolete and use the S25FL064L for the first time. Until now not successfully. I will list the log dump below. Bypass the ID check in iMPACT with XIL_IMPACT_SKIPIDCODECHECK is done. FLASH selection:

I hope that anyone can help me.

INFO:iMPACT - Current time: 28-3-2019 9:49:54

PROGRESS_START - Starting Operation.

'1': SPI access core not detected. SPI access core will be downloaded to the device to enable operations.

INFO:iMPACT - Downloading core file C:/Xilinx/14.7/LabTools/LabTools/spartan6/data/xc6slx150_spi.cor.

'1': Downloading core...

LCK_cycle = NoWait.

LCK cycle: NoWait

done.

'1': Reading status register contents...

INFO:iMPACT:2219 - Status register values:

INFO:iMPACT - 0011 1100 1110 1100

INFO:iMPACT:2492 - '1': Completed downloading core to device.

'1': ID Check passed.

'1': ID Check passed.

'1': Erasing Device.

'1': Using Sector Erase.

'1': Erasing non-volatile quad-enable bit...

'1': Programming Flash.

'1': Reading device contents...

Failed at address, 1293056

'1': Verification Terminated

INFO:iMPACT - '1': Flash was not programmed successfully.

PROGRESS_END - End Operation.

Elapsed time = 278 sec.

1 Solution
lock attach
Attachments are accessible only for community members.

Takahiro,

Thanks to the help by Xilinx, the problem is solved. The solution is to switch off the verify option when starting flash programming.

Daan

Van: TakahiroK_16

Verzonden: maandag 1 april 2019 9:56

Aan: Daan ter Haar - LISMAR

Onderwerp: Re: - S25FL064L trouble

<http://www.cypress.com>

Cypress Developer Community <https://community.cypress.com/?et=watches.email.thread>

S25FL064L trouble

reply from TakahiroK_16<https://community.cypress.com/people/TakahiroK_16?et=watches.email.thread> in Nor Flash - View the full discussion<https://community.cypress.com/message/191645?et=watches.email.thread#191645>

View solution in original post

0 Likes
5 Replies
TakahiroK_16
Employee
Employee
100 replies posted 50 replies posted 25 solutions authored

Hello,

The image you attached is too small to see your settings. Could you send larger one?

When I tested the FL064L with the Spartan 6, I selected S25FL064P, data Width 4.

pastedImage_0.png

And I got log like this.

pastedImage_1.png

Thanks,

Takahiro

0 Likes
lock attach
Attachments are accessible only for community members.

Dear Takahiro,

We use bitstream encryption in our product. Then the choices are limited to data width x1, so we use data width 1 (see attached picture).

Daan

Van: TakahiroK_16

Verzonden: vrijdag 29 maart 2019 7:45

Aan: Daan ter Haar - LISMAR

Onderwerp: Re: - S25FL064L trouble

<http://www.cypress.com>

Cypress Developer Community <https://community.cypress.com/?et=watches.email.thread>

S25FL064L trouble

reply from TakahiroK_16<https://community.cypress.com/people/TakahiroK_16?et=watches.email.thread> in Nor Flash - View the full discussion<https://community.cypress.com/message/191454?et=watches.email.thread#191454>

0 Likes

Hi Daan,

Thanks for the screen capture. I see your Flash selection is the "AT45DB321B" which is not compatible with FL064L. I guess you selected FL064P when you got the iMPACT message in your first post.

Question:

In your first post, the iMPACT outputs:

     '1': Reading device contents...

     Failed at address, 1293056

Is the failure address always same if you try to program multiple times?

Thanks,

Takahiro

0 Likes
lock attach
Attachments are accessible only for community members.

Takahiro,

You are right. Of course I selected FL064P. I have attached images of three impact runs, you can see there the (different) failure addresses.

Daan

Van: TakahiroK_16

Verzonden: maandag 1 april 2019 9:56

Aan: Daan ter Haar - LISMAR

Onderwerp: Re: - S25FL064L trouble

<http://www.cypress.com>

Cypress Developer Community <https://community.cypress.com/?et=watches.email.thread>

S25FL064L trouble

reply from TakahiroK_16<https://community.cypress.com/people/TakahiroK_16?et=watches.email.thread> in Nor Flash - View the full discussion<https://community.cypress.com/message/191645?et=watches.email.thread#191645>

0 Likes
lock attach
Attachments are accessible only for community members.

Takahiro,

Thanks to the help by Xilinx, the problem is solved. The solution is to switch off the verify option when starting flash programming.

Daan

Van: TakahiroK_16

Verzonden: maandag 1 april 2019 9:56

Aan: Daan ter Haar - LISMAR

Onderwerp: Re: - S25FL064L trouble

<http://www.cypress.com>

Cypress Developer Community <https://community.cypress.com/?et=watches.email.thread>

S25FL064L trouble

reply from TakahiroK_16<https://community.cypress.com/people/TakahiroK_16?et=watches.email.thread> in Nor Flash - View the full discussion<https://community.cypress.com/message/191645?et=watches.email.thread#191645>

0 Likes