Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Nor Flash Forum Discussions

AlFe_1631716
Level 1
Level 1
First like received

Hi,

what is the pseudo thermal resistance psi JT of a S25FL064LABNFI013 flash memory?

What is the maximum junction temperature?

Thank you.

0 Likes
1 Reply
AlbertB_56
Moderator
Moderator
Moderator
500 replies posted 50 likes received 250 replies posted

Hello,

Thank you for contacting Cypress Semiconductor

The thermal resistance values for the S25FL064LABNFI013 (8-contact WSON)

  - theta j-a : 34 C/W

  - psi j-t :  1 C/W  (junct. to top-of-case)

  - estim. field voltage :  3.6V (max.)

  - estim. field current :  30mA (max., QIO / QPI mode @ 108MHz)

  - estim. field Pd :  108mW (max)  

  - max. oper. junct. temp. :  88.7C (based @ max operating ambient temp of 85C).

Best regards,

Albert

Cypress Semiconductor Corp.

An Infineon Technologies Company    

0 Likes