Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Nor Flash Forum Discussions

DaNe_4783256
Level 1
First solution authored
Level 1

Hello,

I was hoping to load default values into the memory array, CFI field and protection bits for the S29GL512S12DHE010 for the VHDL simuation model for the S29GL512S. How do I do this? The user manual leaves a lot to be desired and I dont know how to do it. It would be great if one could be created for me. It looks like if I make the UserPreload false, it defaults everything to undefined (U) and I would think that would force me to issue an erase command then send a write command. The test bench calls out these files as constants but I dont see where these files are at all for a different flash part. All I want to do is send write to buffer, and word program commands. I may also want to read commands so having a template of sort that I can modify would be a great help. Unfortunally the provided simulation model to my knowledge doesn't address this at least in a clear, easy to understand way.

Thanks, Dan

0 Likes
1 Solution
2 Replies
DaNe_4783256
Level 1
First solution authored
Level 1

Oops wrong area. Gonna re-ask it in the NOR Flash topic

0 Likes
Roy_Liu
Moderator
Moderator 1000 replies posted 500 solutions authored 5 questions asked
Moderator

Thanks for made post in NOR Flash space, let's refer to that thread

Pre-load simulation model for S29GL512S12DHE010 to an erased condition

Roy Liu
0 Likes