Jan 15, 2023
04:01 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 15, 2023
04:01 PM
Hi,
What is the absolute max operating junction temperature of S25HS512TFANHI01X?
Best Regards,
Kumada
Labels
- Labels:
-
Memory Nor Flash
1 Reply
Jan 25, 2023
10:52 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 25, 2023
10:52 PM
Hello Kumada-san,
Thank you for contacting Infineon Technologies.
The maximum operating junction temperature for the S25HS512TFANHI01X is 89.5 C
based on the following:
theta j-a: 32.7 C/W
max voltage: 2.0V
max current @ 166 MHz: 69 mA
max Pd: 138 mW
max operating ambient temp.: 85 C
Best regards,
Albert
Infineon Technologies