Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Nor Flash Forum Discussions

WoHa_955446
Level 4
Level 4
50 questions asked 100 sign-ins 50 replies posted

Dears.

I’m looking for the QSPI memory which meets the following specification. But I couldn’t find proper cypres PN.

Please give me your recommended part number.

  1. Interface Frequency : 133MHz
  2. Density : 128Mbit or 256MBit
  3. External Reset needed
  4. Interface : QSPI (D0 ~ D3)
  5. Package : WSON 6x5 or FAC024
  6. Operating Voltage : 1.8V

Br,

WonjinHan

0 Likes
1 Solution
AS_36
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi WonjinHan,

Thank you for contacting Cypress Community.

You can use our Product Selector to choose the appropriate part as per your requirements - Product Selector Guide (cypress.com)

As per the mentioned requirements, the most appropriate part for you is S25FS256SAGNFIxxx. You can get the datasheet for S25FS256S device here - S25FS128S/S25FS256S, 1.8 V, Serial Peripheral Interface with Multi-I/O, MirrorBit® Non-Volatile Flas...

Go through the 'Ordering Information' section of the datasheet in order to understand part numbers better.

Hope this answers your question.

Thank you and Regards,

Apurva

View solution in original post

0 Likes
4 Replies
AS_36
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi WonjinHan,

Thank you for contacting Cypress Community.

You can use our Product Selector to choose the appropriate part as per your requirements - Product Selector Guide (cypress.com)

As per the mentioned requirements, the most appropriate part for you is S25FS256SAGNFIxxx. You can get the datasheet for S25FS256S device here - S25FS128S/S25FS256S, 1.8 V, Serial Peripheral Interface with Multi-I/O, MirrorBit® Non-Volatile Flas...

Go through the 'Ordering Information' section of the datasheet in order to understand part numbers better.

Hope this answers your question.

Thank you and Regards,

Apurva

0 Likes

Hello Apurva.

Thank you for your turn-around.

I already used to make it filter with Part Selector but it's impossible to do sorting whether it has external Reset Pin or not.

And also reviewd S25FS256SAGNFIxxx part but If I make IO0 ~ IO3 dedicated for QSPI , I can't use external Reset Pin which is hardware-initialized by external controller.

Do you have any recommended part which has independent external Reset Pin not Alternate function ?

Br,

WonjinHan.

0 Likes
AS_36
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi WonjinHan,

Unfortunately, we do not have an FS-S flash part with a separate RESET# pin. However, please see this below snip from the datasheet that may be useful for you -

pastedImage_1.png

Regards,

Apurva

0 Likes

Hello Apurva.

I appreciate your answer and got your point.

Thanks and regards,

Wonjin Han.

0 Likes