Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

stsmc_4036906
Level 1
Level 1

Is an IBIS model available for S70GL02GT12FHIV10? If not, how do I request one?

3 Replies
AS_36
Moderator
Moderator
Moderator
100 likes received 500 replies posted 250 solutions authored

Hi Steve,

Sincere apologies for the delay in my response.

We have been working on this issue internally, and shall get back to you on this as soon as possible.

Regards,

Apurva

0 Likes
DaBl_4548126
Level 2
Level 2
First solution authored First like received Welcome!

I did find a model for the similar S70GL02GT12FHBV13, however it is only for operation at 3V I/O voltage. I need 1.8V I/O operation. The I/O voltage can be anywhere from 1.65V to VCC(nominally 3.3V). It would be great if they could support at least the 1.8V and 2.5V standards in the IBIS model. See this link: http://https://www.cypress.com/search/all/S70GL02gt?sort_by=changed&f%5B0%5D=meta_type%3Asoftware_to...

0 Likes
lock attach
Attachments are accessible only for community members.

Hi Steve Smith, Dale Blankenship,

Sorry for the delay from our side. We have created IBIS models for both the parts S70GL02GT12FHIV10 and S70GL02GT12FHBV13. Please find them attached to this response.

S70GL02GT12FHIV10: s70gl02gt_a_i_30_r21.ibs

S70GL02GT12FHBV13: s70gl02gt_c_v_18_r21.ibs

Thanks and Regards,

Sudheesh