Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
sash_3755821
Level 1
Level 1
First reply posted First question asked First like given

Hi.

Could you please let me know what is the ESD rating's for below Part.

  • S29GL01GT12TFN01*
0 Likes
1 Solution
Apurva_S
Moderator
Moderator
Moderator
100 likes received 500 replies posted 250 solutions authored

Hi,

Thank you for contacting Cypress Community.

ESD CDM is 750V and ESD HBM is 2.0kV.

Thanks and Regards,

Apurva

View solution in original post

5 Replies
Apurva_S
Moderator
Moderator
Moderator
100 likes received 500 replies posted 250 solutions authored

Hi,

Thank you for contacting Cypress Community.

ESD CDM is 750V and ESD HBM is 2.0kV.

Thanks and Regards,

Apurva

Thank you Apurva.

Can you Please provide the ECCN(Export Control Classification Number) for the below series:

S29GL01GT*

0 Likes

Hi,

The ECCN is 3A991.B.1.A.

Thanks and Regards,

Apurva

Hi Apurva,

S29GL01* series Datasheet( Pg.no 101) DHN and TFN are represented as DHV,FHV and TFV. so is that datasheet Error or valid ordering and moreover Suffix option 'x" is for packaging (0/3) but in some cases represented as "xx".What is that one more "x" represents?.please find below screen shot.

untitled.png

Regards,

Sanathraj Shetty

0 Likes

Hello Sanathraj,

Within the S29GL01GT datasheet, page 101, Table 51.  S29GL-T Valid Combinations for CFI Version 1.5 is incorrect,

as it is certainly a typographical error.   However, it is important to highlight that page 100, Table 50.  S29GL-T Valid

Combinations for CFI Version 1.3 is correct.

A Cypress Defect Tracking (CDT) ticket will be generated to correct the typographical error on page 101,   Table 51.

S29GL-T Valid Combinations for CFI Version 1.5.

In regards to the additional "X" within the suffix, it is just an additional character, with no significant meaning.

There should be only one "X", as the packing option is either "1" or "3" only.

Hope this helps...

Best regards,

Albert

Cypress Semiconductor