- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi everyone,
we use the S25HL512T with QUAD-SPI interface and find some issue about QPI read.
some test pattern as follow:
Does somebody encounter the same problem?
- Labels:
-
Memory Nor Flash
- Tags:
- QUAD-SPI Read Issue
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Ken
Are you performing the program operation across page boundaries? I would like to inform you that the default size of the program buffer is set to 256, means page boundaries occur at every 256th memory location. If the page boundary is crossed during the page program operation, the address gets wrapped and programming starts from the starting of that particular page. Can you confirm that your program operation is not crossing page boundaries?
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
We tested these addresses
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Ken
I would like to point out that there is difference between Quad SPI mode and QPI mode.
Quad mode is enabled by the below configuration register bit
QPI mode is enabled by the below configuration register bit
Could you please confirm which mode are you using?
Regards.
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
We set the output drive impedance register to 001 (120 ohms), which is normal.
Who can help explain the details about the settings?
Why does it cause it to read the failed value (read a byte is 0x0F or 0xF0)?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Ken
IOIMPD[2:0] bits are required to select the IO driver output impedance. It is used to adjust the drive strength to meet the systems signal integrity requirements.
- Can you please tell how are you confirming that the program operation was successful? Are you capturing the SPI signals?
- If yes, can you provide the screenshots of the waveform for page program as well as read operations?
- Also provide the exact sequence of commands that you are following.
- How many devices are showing this behavior?
- Is it possible that you may have performed excessive number of program/erase operations on the particular memory location being used for testing, such that you may have exhausted all the P/E cycles for that particular location?
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
3. I can provide the sequence, if we don't configure the 120 ohm impedance.
The reading process became abnormal, even read ID command, because it has an 0x0F value.
the sequence
printf("Impedance\r\n");
S25HS_Write_Enable();
Data = S25HS_Read_Reg(REG_ADDR_CONG4);
Data |= (1 << 5); //used 120 ohm
S25HS_Write_Reg(REG_ADDR_CONG4, Data);
S25HS_Read_Reg(REG_ADDR_CONG4);
printf("QPI\r\n");
//Set QPI mode and 4 bytes addressing for 512M bit = 64 MB
Data = S25HS_Read_Reg(REG_ADDR_CONG2);
S25HS_Write_Enable();
Data = (Data | 0xC0); // 4 bytes
//Data = (Data | 0x40); // 3 bytes
S25HS_Write_Reg(REG_ADDR_CONG2, Data);
S25HS_Busy4_Wait();
S25HS_32Read4_Reg(REG_ADDR_STAT1);
S25HS_Write4_Enable();
S25HS_32Read4_Reg(REG_ADDR_STAT1);
printf(" Erase \r\n");
//S25HS_Erase_Sector(0x03F00000);
S25HS_Erase_Block(0x03FF0000);
//S25HS_Erase_Chip();
S25HS_Busy4_Wait();
printf("D %08X D\r\n", S25HS_QuadSPI_Read_Test256());
printf(" Read \r\n");
TIM10->CNT = 0;
S25HS_QuadSPI_Read_Test256();
TS = TIM10->CNT;
printf("~~~~ TS :%d us\r\n", TS);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Kent_Lee
Apologies for the delay in responding.
We would need some more information.
- How many chips showed this issue? Did you try to perform A-B-A test to see whether the issue follow with chip or board?
- Can you try to use FAST READ other than QPI mode I/O read to see whether it’s the same behavior or not?
- Did you try to perform READ_ID command in SPI mode or QPI mode? If the issue happened in QPI mode, can you try to restore to SPI mode and try again? Normally the RDID command should work in all cases without configurations.
Regards.