Hello,
I am using the S25FS512SDSBHV213 in serial SPI mode. Quad is not available on the nrf52832 processor. The only commands that seem to have effect are volatile ones, all non-volatile commands appear to fail silently. I only have the one custom PCB for another few weeks, is there any other tests I can run to see if it is just a bad IC, or if it is my firmware?
Code Run |
---|
//Set 4 byte mode static uint8_t four_byte_mode[] = {0xB7}; static uint8_t four_byte_mode_len = 1; ////Read from Any register static uint8_t rdar_addr[] = {0x65, 0x00, 0x00, 0x00, 0x00 }; //Reads from any register static uint8_t rdar_addr_len = 5; static uint8_t rdar[64]; static uint8_t rdar_len = 5+1; //write length plus actual register ////Write to Config Register 2 Non-Volatile static uint8_t cr2nv[] = {0x71, 0x00, 0x00, 0x00, 0x03, 0x88}; //writes to CR2NV , bit7=4-byte addressing, 6=QSPI, 5=IO3Reset,4=RFU, 3-0 = Read Latency static uint8_t cr2nv_len = 6; //Write Enable Command static uint8_t write_en_cmd[] = {0x06}; //addr 06 static uint8_t write_en_cmd_len = 1; static void memory_read_register(uint32_t address, char * str, uint8_t len) { if(memory_wait_until_ready() == false) { NRF_LOG_ERROR("Flash timed out before we could erase everything"); NRF_LOG_FLUSH(); } set_command_address(rdar_addr,address); spi_read(FLASH_SSEL_PIN,rdar_addr,rdar_addr_len,rdar,len); NRF_LOG_RAW_INFO("%s ",str); uint8_t i; for(i=0; i < len; i++) NRF_LOG_RAW_INFO("0x%02x ",rdar); NRF_LOG_RAW_INFO("\r\n"); NRF_LOG_FLUSH(); } void memory_init (void) { ret_code_t err_code; uint8_t i; for(i=0; i < 4; i++) who_am_i = 0; //read the information about the flash to make sure it is the correct one spi_read(FLASH_SSEL_PIN,who_am_i_addr,who_am_i_addr_len, who_am_i, who_am_i_len); NRF_LOG_DEBUG("Indentification info should match 0x01,0x02,0x20 : 0x%02x,0x%02x,0x%02x ", who_am_i[1], who_am_i[2], who_am_i[3]); //Set ourselves in 4-byte addressing mode spi_write(FLASH_SSEL_PIN,write_en_cmd, write_en_cmd_len); spi_write(FLASH_SSEL_PIN,four_byte_mode, four_byte_mode_len); nrf_delay_ms(100); //Permanently set ourselves into 4 byte mode spi_write(FLASH_SSEL_PIN,write_en_cmd, write_en_cmd_len); spi_write(FLASH_SSEL_PIN,cr2nv, cr2nv_len); nrf_delay_ms(100); //flash memory timer err_code = app_timer_create(&flash_erase_timer_id, APP_TIMER_MODE_SINGLE_SHOT, flash_erase_timeout_handler); APP_ERROR_CHECK(err_code); //read from our status registers spi_read(FLASH_SSEL_PIN,sr1v_addr,sr1v_addr_len,sr1v,sr1v_len); NRF_LOG_INFO("SR1: %d",sr1v[2]); spi_read(FLASH_SSEL_PIN,sr2v_addr,sr2v_addr_len,sr1v,sr1v_len); NRF_LOG_INFO("SR2: %d",sr1v[2]); spi_read(FLASH_SSEL_PIN,cr1v_addr,sr1v_addr_len,sr1v,sr1v_len); NRF_LOG_INFO("CR1: %d",sr1v[2]); memory_read_register(0x00800000, "SR1:", 8); memory_read_register(2, "CR1NV:", 8); memory_read_register(3, "CR2NV:", 8); memory_read_register(4, "CR3NV:", 8); memory_read_register(5, "CR4NV:", 8); memory_read_register(0x00800002, "CR1:", 8); memory_read_register(0x00800003, "CR2:", 8); memory_read_register(0x00800004, "CR3:", 8); memory_read_register(0x00800005, "CR4:", 8); memory_read_register(0x00800040, "PPBL:", 8); spi_write(FLASH_SSEL_PIN,write_en_cmd, write_en_cmd_len); memory_read_register(0x00800000, "SR1:", 8); memory_read_ppbr(0, "PPBR:", 16); NRF_LOG_FLUSH(); FLAG_FLASH_FINISHED_ERASING = 0; head_pointer = 0; tail_pointer = 0; } |
Results |
---|
<debug> app: Indentification info should match 0x01,0x02,0x20 : 0x01,0x02,0x20 <info> app: SR1: 0 <info> app: SR2: 0 <info> app: CR1: 0 SR1: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 CR1NV: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 CR2NV: 0x00 0x00 0x00 0x00 0x00 0x00 0x08 0x08 CR3NV: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 CR4NV: 0x00 0x00 0x00 0x00 0x00 0x00 0x10 0x10 CR1: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 CR2: 0x00 0x00 0x00 0x00 0x00 0x00 0x88 0x88 CR3: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 CR4: 0x00 0x00 0x00 0x00 0x00 0x00 0x10 0x10 PPBL: 0x00 0x00 0x00 0x00 0x00 0x00 0x01 0x01 SR1: 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 PPBR: 0x00 0x00 0x00 0x00 0x00 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF |
Hello,
Thank you for contacting Cypress Community Forum. We have received your inquiry and currently reviewing the case. We will get back to you as soon as we find the resolution.
Have a wonderful day
Regards,
Bushra
Hello,
What exact non-volatile command is failing? The correct right device IDs being read and also the register values don't look too wrong.
Thank you
Regards,
Bushra
Hi Bushra,
I'm writing cr2nv[] by sending this command:
cr2nv[] = {0x71, 0x00, 0x00, 0x00, 0x03, 0x88}; //writes to CR2NV
But afterwards, CR2NV still remains at 0x80.
CR2 volatile is at 0x88 because the 4-byte mode command worked.
static uint8_t four_byte_mode[] = {0xB7};
I have also tried writing regular flash through the command {0x06} then {0x12,0x00,0x00,0x00,0x00, 0x01}, but readbacks {0x13,0x00,0x00,0x00,0x00} only give 0xFF.
Thank you
Hi Bushra,
Is there a "global flash write" enable command for this chip? I do not see such information in the datasheet.
Hello,
Did you send the Write Enable command (06h) before writing to the registers or programming to the flash?
Thank you
Regards,
Bushra
Hi Bushra,
Yes, I send the single character {0x06} followed by {0x71, 0x00, 0x00, 0x00, 0x03, 0x88};
But CR2NV stays at {0x08} instead of changing
Thank you very much
Hello
Please send us the logic analyzer traces.
Thank you
Regards,
Bushra
Hello,
We are still waiting for logic analyzer traces to debug the issue.
Thank you
Regards,
Bushra
Hello Bushra,
I am awaiting for a second PCB to arrive. I do not have good access to place logic analyzer probes on the current device.
I ordered the same flash in a different package and hand wired it up to a development kit. I got even worse replies out of the flash, even when responding to the ID request command. I was able to take pictures of that, but I do not think they will be useful in troubleshooting.
Thanks