Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
noha_3407421
Level 3
Level 3
Distributor - TED (Japan)
First like received 10 replies posted 10 questions asked

Hi,

Customers are using S29GL064S80TFIV10.

After issuing the CFI Query command to read the CFI region, issue the CFI Exit command to return to normal.

  *CFI Exit command = Write 0xF0.

Q.

What is the maximum time (ns) for returning from the query mode to the normal state?

--- Question background ---

After issuing the CFI Exit command, reading outside the CFI area will lead to a value different from the expected value.

Therefore, I want to check the time between issuing the CFI Exit command and returning to normal state.

---------------------------

Best Regards,

Harukawa

0 Likes
1 Solution
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi Harukawa-san,

You will only need to match the timings as per  the datasheet in figures 28 and 29 respectively.

pastedImage_0.png

When you write the exit command the internally there is a reset done. The reset command does not take much time. The reset command just clear status (if error occured ) or exit CFI (or other ASO) and it is done immediately. Therefore you don't need any additional delay after reset command if you meet the timings in Figure 28 or 29.

Thanks,

Pradipta.

View solution in original post

0 Likes
1 Reply
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi Harukawa-san,

You will only need to match the timings as per  the datasheet in figures 28 and 29 respectively.

pastedImage_0.png

When you write the exit command the internally there is a reset done. The reset command does not take much time. The reset command just clear status (if error occured ) or exit CFI (or other ASO) and it is done immediately. Therefore you don't need any additional delay after reset command if you meet the timings in Figure 28 or 29.

Thanks,

Pradipta.

0 Likes