Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions

Sort by:
HiKu_1337496
Non Volatile RAM (F-RAM & NVSRAM)
Hi there, Can you tell me the baking conditions for FM25CL64B-GTR? What we would like to know is as follows:・High Temperature Baking Conditions・Low Te... Show More
ARVA
Non Volatile RAM (F-RAM & NVSRAM)
Does anyone have  radiation test data on FRAM CY15B102Q (e.g. full part number CY15B102Q-SXM or similar) or on this part family? Looking for gamma “to... Show More
Jay_Rotondo
Non Volatile RAM (F-RAM & NVSRAM)
1.  With respect to the NVSRAM (CY14B256LA-SP25XIT) what it the structure/impedance between the power pin(s), VCC, and the storage cap Vcap.2.  If giv... Show More
JpW_810898
Non Volatile RAM (F-RAM & NVSRAM)
Hi, Soft Error Rate discussion on NvRAM in thread from 10/16/2018 06:00PM provided a Report file to the discussion initiator. Are similar SEU/SEL repo... Show More
Sergey25
Non Volatile RAM (F-RAM & NVSRAM)

The marking

СY152D3

A 600402

CYP2101

corresponds to the product CY15B104QN-50SXI ?

GirijaC
Non Volatile RAM (F-RAM & NVSRAM)
Check out the Article "Ensuring fail-safe data storage in battery-powered IoT sensor nodes". In this article, we will examine the often neglected but ... Show More
GirijaC
Non Volatile RAM (F-RAM & NVSRAM)
Infineon Linux SPI RAM Memories Drivers have been ported to Linux kernel 5.4.40. These drivers are available at GitHub. To download the Drivers, click here... Show More
EricC_76
Non Volatile RAM (F-RAM & NVSRAM)
The focus in this F-RAM video is on ADAS for automotive applications where instant data capture is a critical feature for event data recorders. Learn ... Show More
EricC_76
Non Volatile RAM (F-RAM & NVSRAM)
When failure is not an option, count on Cypress’ Excelon F-RAM memory to store and protect your mission-critical data.Download our Application Note on... Show More
GernotH_31
Non Volatile RAM (F-RAM & NVSRAM)
This blog is to announce the availability of a new software driver for STM32 family members that include ST's latest OctoSPI controller block, i.e.   ... Show More
Forum Information

Non Volatile RAM (F-RAM & NVSRAM)

Non-volatile RAM forum discusses Technology such as F-RAM and nvSRAM, which combine non-volatile data storage up to 16Mbit density with the high performance of RAM. These low-power memories offer high endurance, high data retention and instant non-volatility without external battery back-up, enabling system reliability and cost reduction.