Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions

Sort by:
burgdani
Non Volatile RAM (F-RAM & NVSRAM)
We have an FM25L16B in our product. I want to know how long it takes the memory chip to write one byte to the cell of the FRAM after it has been trans... Show More
_Frank_
Non Volatile RAM (F-RAM & NVSRAM)
Hello, AC characteristics for SPI FRAM (FM25CL64B) is based on signal rise/fall times of 5ns, which includes CLK signal as well. What is the max. acce... Show More
MAO
Non Volatile RAM (F-RAM & NVSRAM)

Regarding some FRAM -> Please explain why WP and Reset are now recommended for VDD connection.

MAO
Non Volatile RAM (F-RAM & NVSRAM)

Regarding the backup of nvSRAM, is it possible to control it with SW other than when the power is turned off?

Bbbbgg2023
Non Volatile RAM (F-RAM & NVSRAM)

CY14B101PA-SFXIの下記仕様をお教えください。
保管環境と動作環境の各仕様(温度、湿度、耐振動、場所)

GlenLee
Non Volatile RAM (F-RAM & NVSRAM)

Sir,

  Is possible have design guidle of Parallel  NVRAM ?

  Thanks.

 

Glen

durgeshg
Non Volatile RAM (F-RAM & NVSRAM)
Could you please provide us the latest REACH-233, ROHS, TSCA coc’s and Material Declaration Sheets for the below parts # FM22L16-55-TG FM22L16-55-TGTR Show More
Andrei_C
Non Volatile RAM (F-RAM & NVSRAM)
I've run into a problem with some FM25CL64B-GA chips in a new device. To initialize the FRAM (not trusting the factory default values), I read a speci... Show More
五五
Non Volatile RAM (F-RAM & NVSRAM)
The program cannot read and write after porting (after repeated testing), the data register assignment of SPI cannot be changed, the read and write ti... Show More
Cosmo_Little
Non Volatile RAM (F-RAM & NVSRAM)
Sirs, I have been chasing an intermittent write problem with the CY15B104Q-SPI 1/- Hardware. 4off memories are connected to SPI2 on the dsPIC33E512GM3... Show More
Forum Information

Non Volatile RAM (F-RAM & NVSRAM)

Non-volatile RAM forum discusses Technology such as F-RAM and nvSRAM, which combine non-volatile data storage up to 16Mbit density with the high performance of RAM. These low-power memories offer high endurance, high data retention and instant non-volatility without external battery back-up, enabling system reliability and cost reduction.