Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions
Regarding some FRAM -> Please explain why WP and Reset are now recommended for VDD connection.
Regarding the backup of nvSRAM, is it possible to control it with SW other than when the power is turned off?
Sir,
Is possible have design guidle of Parallel NVRAM ?
Thanks.
Glen
Hello,
I tried to find the technical support for Fujitsu MB85RC1MT. After searching on their website, I was guided to Infineon website. I think the product might be transferred to Infineon.
Can anyone confirm if it is true?
Thanks!
Crane
Show LessHello Community,
I am new to Cypress-Infineon F-RAM products. To start experimenting on CY15FRAMKIT-002, I got STM Nucleo STM32L433RC-P development board and the installed the KEIL ARM uVision 5.37.0.0 as reported on document 002-23147 Rev. *A: "Infineon-CY15FRAMKIT-002_Kit_User_Guide-UserManual-v01_00-EN.pdf". However, pack installer uVision seems no (longer) to recognise this particular board. Did anyone had similar experience and can help me on moving a bit forward? Thanks.
Show Less
What is the minimum Vcap voltage for Autostore in CY14B101KA-SP25XI?
Hello,
A customer wants to use the CY14B116K with the RealTimeClock feature disabled.
The following pins on the 44-TSOP package
Xout(21), Xin(22), VRTCcap(24), VRTCbat(23), and INT(1) are unconnected.
Are there any other necessary settings on the software?
Should the OSCEN bit in the calibration register( 0x1FFFF8) be written to "1" (Disable Oscillator) by the user?
If so, is this register non-volatile? (Once you write "1" to the register, it will be retained even after power-off.)
MPN: CY14B116K-ZS25XI
Best reards,
Naoaki Morimoto
Show Lesslpc单片机 移植后程序无法读写(经过反复测试),SPI的数据寄存器赋值无法更改,数据手册上的读写时序一致,这是为什么,有什么需要注意的
Please let me know the longevity of CY14B108N. Is It available for next 20 years, or let us know when this product will be obsolete
Hi,
Can F-RAM products be used in vacuum or near-vacuum environment?
not in space, but in the facility on the ground.
Regards,
Junichi Nagata
Show Less