Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions
I think the FM28V202A has a capacity of 2Mbit, but even in the simulation model
Is it possible to simulate full area access for 2Mbit?
If you use a simulation model, please let us know if there are any restrictions on driver development.
(For example, access to a specific area can only be simulated, etc.)
Show LessDo you have any test data available for radiation exposure and SEE/SEU/SEL?
Since there is a risk that the development schedule will be delayed, we are considering whether there is a way to check the operation of FM28V202A-TGTR in advance.
Thank you
Show Less
Can anyone please confirm ESD(HBM)ratings and MSL for below part numbers
> CY14E256LA-SZ25XI*
>CY14E256LA-SZ45XI*
Hi,
I´m looking for MTBF or FIT-Rate for CY15B064Q
thank you in advance
kind regards
Thomas
Dear technical team,
I am going to set up FM22L16 and FM28V202A. Can you guide me, please which microcontroller you suggest for these memories?
Thanks!
Show LessHi,
I have interfaced cy14b101i-sfxi with my NXP Processor. While checking the read write operation, rtc, i am not getting any data? Can you help me to resolve the issue?
Attaching the interface diagram of my design? Please let me know the connections are correct or not? Also, what will be the status of HSB pin my design?
Regards
Hemant
Show LessHI,
I am using CY15B064Q-SXE IC as it suits my requirement.
In the product spec it was written that minimum operating temperature is -40 deg.
But in datasheet it is mentioned that, the operating temperature range when powered up is (-50 deg).
Which temperature should i consider.
What is the difference between them.
Thanks & Regards
Naresh
Show Less