Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions
text.format{('custom.tabs.no.results')}
Do you have any idea why the first byte of the ID is always 0 when read in QPI mode? If I remove power completely from the F-RAM it resets back to SPI mode and the ID is then read correctly with a 0x50 for the first byte. Just curious if anyone else has seen this.
Hello, I would like to ask you whether the empty status of FM18W08-SG is full address FF or full address 00. Thank you.
Does anyone have a communication example with CY15B116QN? I have no problem getting a stable reading from registers like Device ID, but very random luck with reading and writing. No problem with smaller-size FRAMs. Supplying 3.3V off the Atmel SAMD21 chip via standard SPI at 8MHz. Thank you.
WRITE to F-RAM works fine only once, right after the multi-byte READ command it stops writing data, and not a single subsequent iterations work.
PS: WP is connected to VDD.
Show LessHello,
AC characteristics for SPI FRAM (FM25CL64B) is based on signal rise/fall times of 5ns, which includes CLK signal as well.
What is the max. acceptable clock rise/fall time, supported by the device?
Thanks in advance
Frank
We have an FM25L16B in our product. I want to know how long it takes the memory chip to write one byte to the cell of the FRAM after it has been transferred to the memory chip via SPI. I need this information to calculate the probability that a power interruption will interrupt this write cycle.
A similar question was asked in https://community.infineon.com/t5/Non-Volatile-RAM-F-RAM-NVSRAM/FRAM-access-time/td-p/119910, but the write access time was not given by @PradiptaB_11 .
Thanks,
Daniel
Show LessRegarding some FRAM -> Please explain why WP and Reset are now recommended for VDD connection.
Regarding the backup of nvSRAM, is it possible to control it with SW other than when the power is turned off?
CY14B101PA-SFXIの下記仕様をお教えください。
保管環境と動作環境の各仕様(温度、湿度、耐振動、場所)
Sir,
Is possible have design guidle of Parallel NVRAM ?
Thanks.
Glen