Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions

ShSe_1328206
Non Volatile RAM (F-RAM & NVSRAM)
Regarding CY14B108n-ZSP25XI, Package is PG-TSOP-54. is the inside of the IC filled with resin?In order to confirm that the BEOL change does not affect... Show More
ShSe_1328206
Non Volatile RAM (F-RAM & NVSRAM)
Regarding CY14B108N-ZSP25XI , PG-TSOP 54 Is the inside of the IC filled with resin?In order to confirm that the BEOL change does not affect the impact... Show More
Yi0228
Non Volatile RAM (F-RAM & NVSRAM)

Excuse me,What is the empty state of the FM25V series? All 00 or all FF?

MAO
Non Volatile RAM (F-RAM & NVSRAM)

Are there any soldering reflow conditions for this model number?

easl
Non Volatile RAM (F-RAM & NVSRAM)
fm22l16-55-TG
solved msg Solved
Hi. Can assist to advice what is the suffix "Q1" behind the lot no : 612300149Q1 I have some other lot no which doesn't have the Q1, Example: Lot no: ... Show More
GoKo_4683011
Non Volatile RAM (F-RAM & NVSRAM)
FM28V202A
solved msg Solved
Dear technical team, Could you guide me please with this question? I am working with parallel memory FM28V202A that is connected to Arduino DUE. When ... Show More
ctiangho
Non Volatile RAM (F-RAM & NVSRAM)
Saw some post that mentioned there is no CMOS in the F-ram, may i know if the part is consider rad tolerance or harden? is there SEL test result to st... Show More
AndyWang
Non Volatile RAM (F-RAM & NVSRAM)
Hello Cypress team, I have a question about using Linux-SPI-NOR driver to access NVSRAM and read/write data to it. I have refered this commit. https://community.infineon.com/t5/Non-Volatile-RAM-F-RAM-NVSRAM/linux-support-for-CY14V101QS/td-p/337270... Show More
jklofczynski
Non Volatile RAM (F-RAM & NVSRAM)
Hi Guys, May I know the difference between FM24CL64B-G and FM24CL64B-G2TR please? Not asking about TR, but "2" What exactly this "2" stands for?   Tha... Show More
saito
Non Volatile RAM (F-RAM & NVSRAM)
Dear Sir or Madam, I am using CY15B108QN-40SXI(Blank/T) in our product.Please provide RoHS Certificate(2011/65/EU, (EU)2015/863) for CY15B108QN-40SXI(... Show More
Forum Information

Non Volatile RAM (F-RAM & NVSRAM)

Non-volatile RAM forum discusses Technology such as F-RAM and nvSRAM, which combine non-volatile data storage up to 16Mbit density with the high performance of RAM. These low-power memories offer high endurance, high data retention and instant non-volatility without external battery back-up, enabling system reliability and cost reduction.