Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions

Recent discussions

Sort by:
varun
Non Volatile RAM (F-RAM & NVSRAM)
Hey guys, I see FM24C16-P(8 pin DIP) is obsolete on digikey/mouser. I found an alternative FM24C16C-G which is a 8 pin soic . I just wanted to confirm... Show More
pia371
Non Volatile RAM (F-RAM & NVSRAM)
Hello,  I am in need of a IC FRAM 8Mb SPI 20MHz 8GQFN memory. I planned on using the Infineon part #CY15B108QI-20LPXI, but it is out of stock everywhe... Show More
tacq
Non Volatile RAM (F-RAM & NVSRAM)
We have seen the following situtation when using a CY15B104Q-SXI which is accessed by an FPGA on a board with stable power up timing. After a an opera... Show More
peakjohn
Non Volatile RAM (F-RAM & NVSRAM)
Dears :      I want to select a Pin to Pin replacement P/N of FM24CL64B-GTR      It seems CY15E064J-SXA is the best choice      looking from descripti... Show More
NaMo_1534561
Non Volatile RAM (F-RAM & NVSRAM)
FRAMのシミュレーションモデルを使用してQuartus16.1環境にてコンパイルを実施したところ、以下のエラーメッセージとなりました。Error (10106): Verilog HDL Loop error at FM28V202.v(161): loop must terminate with... Show More
saikrishna
Non Volatile RAM (F-RAM & NVSRAM)
FM25L16B-GTR
Solved

Hi ,

This sai i required FM25L16B-GTR component latest certificates are required  REACH and ROHS certificates please share me.

MAO
Non Volatile RAM (F-RAM & NVSRAM)
Regarding the FRAM reset method, it seems that there are two methods, hardware reset / software reset, but please give us information on each reset co... Show More
jchristiansen
Non Volatile RAM (F-RAM & NVSRAM)
Can anyone tell me about the status of CY14B256LA-SZ25XIT ? I am being told from Mouser that it is EOL, but on your website it says active and preferr... Show More
Badger429
Non Volatile RAM (F-RAM & NVSRAM)
I need to find a replacement for FM25L04-G. What is the difference between FM25L04B-G and CY15B004Q-SXA? I need a solution for the next 5+ years. Show More
RicardoALFCG
Non Volatile RAM (F-RAM & NVSRAM)
Hello,    I have been using FM25V10 for a long time, however, and due to the shortage, I had to replace this FRAM to a semi-compatible one which is th... Show More
Forum Information

Non Volatile RAM (F-RAM & NVSRAM)

Non-volatile RAM forum discusses Technology such as F-RAM and nvSRAM, which combine non-volatile data storage up to 16Mbit density with the high performance of RAM. These low-power memories offer high endurance, high data retention and instant non-volatility without external battery back-up, enabling system reliability and cost reduction.