Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions

Sort by:
KaKi_1384211
Non Volatile RAM (F-RAM & NVSRAM)

Hi

CY14B101Q2A-SXIの推奨洗浄条件を教えてください。

Thanks and regards,

rust_4710131
Non Volatile RAM (F-RAM & NVSRAM)
As the datasheet "001-84499_FM25V10_1_Mbit_128K_X_8_Serial_SPI_F_RAM.pdf" describes :The read access is as on the attached picture.So Bit 23 (the 24th... Show More
Cosmo_Little
Non Volatile RAM (F-RAM & NVSRAM)
Dear Sirs,  I have just started to use these FRAM memories. My test software for writing and reading is working 99% of the time.Occasionally I get a c... Show More
GernotH_31
Non Volatile RAM (F-RAM & NVSRAM)
Sometimes it is useful to have a simple and easy-to-use development & test platform at hand. The popular Raspberry Pi platform meets these needs. It i... Show More
WaCh_4680201
Non Volatile RAM (F-RAM & NVSRAM)
Dear Cypress team,I wonder if there is any compatible driver for this device at the space of U-Boot,and U-Boot is release of 2016.07 on ARM platform.T... Show More
HA_4701186
Non Volatile RAM (F-RAM & NVSRAM)
Hello,I'm trying to read the device ID in FM25V20A-PG by sending 1001 1111b using an Arduino nano.The problem is that all I get back is 0xFF on the MI... Show More
MiKr_4700096
Non Volatile RAM (F-RAM & NVSRAM)
Hello community,is there any Chance to replace a 5V SRAM 1to1 with the FM28V100 without the levelshifting things?If i will reduce the circuit Voltage ... Show More
ToAz_4396196
Non Volatile RAM (F-RAM & NVSRAM)
Hello,What is the technology size for the FRAM CY15B102Q?  Also, has this part (or similar FRAM parts) been tested for Single Event Upsets and Single ... Show More
BrLe_4684416
Non Volatile RAM (F-RAM & NVSRAM)
Hi,We are currently experiencing high rates of data corruption in a CY15B104Q-LHXI device on our design.  We see corruption occur only when we write a... Show More
RaHa_4444161
Non Volatile RAM (F-RAM & NVSRAM)
I am using a CY14B101PA, NvRAM/RTC device.I remove the RTC backup battery. After powerup, I see the OSCF and BPF asserted. I clear them and wait 10 ms... Show More
Forum Information

Non Volatile RAM (F-RAM & NVSRAM)

Non-volatile RAM forum discusses Technology such as F-RAM and nvSRAM, which combine non-volatile data storage up to 16Mbit density with the high performance of RAM. These low-power memories offer high endurance, high data retention and instant non-volatility without external battery back-up, enabling system reliability and cost reduction.