Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions

CraigEVD
Non Volatile RAM (F-RAM & NVSRAM)

What are the MTBF / FIT rate data for part numbers S29GL512T12DHN020 and CY15B102QN-50SXET?

Thank you

Craig

jane
Non Volatile RAM (F-RAM & NVSRAM)
We used FM22L-16-55-TG. The control chip matched is 10M08SCE144I7G.  During use, it was found that the data written to FM22L-16-55-TG had been accide... Show More
Sergey25
Non Volatile RAM (F-RAM & NVSRAM)

The marking

СY152D3

A 600402

CYP2101

corresponds to the product CY15B104QN-50SXI ?

Krzysztof
Non Volatile RAM (F-RAM & NVSRAM)
Hello, What is the difference between FM25C160B-GTR vs FM25C160B-GA1TR? What means "A1"?   BR Krzysztof Show More
Nelson
Non Volatile RAM (F-RAM & NVSRAM)
The data I saved in FRAM is 0-255. An error occurred when I read data from FRAM using DMA and SPI, as shown in the figure above. But this error ha... Show More
NaMo_1534561
Non Volatile RAM (F-RAM & NVSRAM)
Hello, I have a question about Auto Store and Recall function of nvSRAM.According to the data sheet, when the voltage (Vcc) drops to the threshold (Vs... Show More
NaMo_1534561
Non Volatile RAM (F-RAM & NVSRAM)
Hello, Customers are considering replacing current parts with new parts. 1) The CY14B116M has an RTC function, but this function will be not used.The ... Show More
raghav
Non Volatile RAM (F-RAM & NVSRAM)
dear cypress tech support team, i am using cypress CM22L16 fram with my ti microcontroller 28379d. while writing the data in the dq bits paralelly aft... Show More
DanCharles
Non Volatile RAM (F-RAM & NVSRAM)

Ferroelectric HZO film is used below the gate. I would like to purchase some devices that use this material

CLFu
Non Volatile RAM (F-RAM & NVSRAM)
Hi,   I am looking for "WM72016-6" which is the 16Kbit Secure F-RAM Memory with Gen-2 RFID. Is the WM72016-6 product still available?  If no, any new ... Show More
Forum Information

Non Volatile RAM (F-RAM & NVSRAM)

Non-volatile RAM forum discusses Technology such as F-RAM and nvSRAM, which combine non-volatile data storage up to 16Mbit density with the high performance of RAM. These low-power memories offer high endurance, high data retention and instant non-volatility without external battery back-up, enabling system reliability and cost reduction.