Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Non Volatile RAM (F-RAM & NVSRAM) Forum Discussions

MAO
Level 4
Level 4
100 sign-ins 25 replies posted 50 questions asked

Regarding some FRAM -> Please explain why WP and Reset are now recommended for VDD connection.

0 Likes
1 Solution
NaMo_1534561
Level 5
Level 5
100 replies posted 100 sign-ins 50 replies posted

If the logic is floating without connecting to VDD, the transistor may operate halfway and the voltage may not be fixed at the ViL or ViH value due to leakage current generation, etc., and may become indefinite (not recognized as High or Low).
Therefore, it is necessary to connect to VDD to fix the logic or add an external pull-up of about 3 to 10K.

View solution in original post

1 Reply
NaMo_1534561
Level 5
Level 5
100 replies posted 100 sign-ins 50 replies posted

If the logic is floating without connecting to VDD, the transistor may operate halfway and the voltage may not be fixed at the ViL or ViH value due to leakage current generation, etc., and may become indefinite (not recognized as High or Low).
Therefore, it is necessary to connect to VDD to fix the logic or add an external pull-up of about 3 to 10K.

This widget could not be displayed.