Minimum voltage required at VCAP pin

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MiNe_85951
Level 7
Level 7
Distributor - TED (Japan)
50 likes received 500 replies posted 50 solutions authored

We confirm for minimum voltatge required at VCAP of nvSRAM.

Minimum voltage required at VCAP pin to complete AutoStore?

Answers were listed on the above link.
"The minimum voltage at VCAP pin for proper circuit operation is 2 V."

Is this answer similar to +3.3V and +5.0V products?

If so,

I = Q / t
Q = CV

From the above equation,
We understand that recommended values of VCAP capacitors for +3.3V and +5.0V products are different.
However, the recommended values are not distinguished in the data sheet.

0 Likes
1 Solution
ShivendraSingh
Employee
Employee
25 solutions authored 50 replies posted 10 solutions authored

Hi Masashi-san,

The minimum voltage on VCAP to complete the AutoStore cycle is the same for both 3V and 5V nvSRAM parts. This is because nvSRAM internal core voltage is regulated to a constant core voltage for both 3V and 5V VCC.

Rgds,

Shivendra

View solution in original post

0 Likes
3 Replies
Anonymous
Not applicable

Hello,

Could you let me know the full MPN of the part you are referring to?

Thanks,

Nada

0 Likes
MiNe_85951
Level 7
Level 7
Distributor - TED (Japan)
50 likes received 500 replies posted 50 solutions authored

Nada-san,

We were confirm to find the minimum store processing voltage of CY14E256LA - SZ45XI(+5V product).

As I was looking into this community, I found a link with an above answer.

Assuming the above answer is correct, I confirm for the data sheet of other products.

For example, CY14MB064Q1B/CY14MB064Q2B with 3.3V and 5V products.

Although this product has different voltage, the value of Vcap is specified with the same value.

So, it has led to this question.

We would like to confirm that this minimum voltage is common to all products(+3.3V and +5V).

Regards,

Masashi

0 Likes
ShivendraSingh
Employee
Employee
25 solutions authored 50 replies posted 10 solutions authored

Hi Masashi-san,

The minimum voltage on VCAP to complete the AutoStore cycle is the same for both 3V and 5V nvSRAM parts. This is because nvSRAM internal core voltage is regulated to a constant core voltage for both 3V and 5V VCC.

Rgds,

Shivendra

0 Likes