- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
A customer wants to use the CY14B116K with the RealTimeClock feature disabled.
The following pins on the 44-TSOP package
Xout(21), Xin(22), VRTCcap(24), VRTCbat(23), and INT(1) are unconnected.
Are there any other necessary settings on the software?
Should the OSCEN bit in the calibration register( 0x1FFFF8) be written to "1" (Disable Oscillator) by the user?
If so, is this register non-volatile? (Once you write "1" to the register, it will be retained even after power-off.)
MPN: CY14B116K-ZS25XI
Best reards,
Naoaki Morimoto
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @NaMo_1534561 ,
>When you are not using the RTC functionality in an nvSRAM with RTC, the RTC-related pins of the part (XIN, XOUT, VRTCcap, and VRTCbat) must be left floating as already you have pointed out. Also, you must ensure that the RTC oscillator is disabled by setting the OSCEN bit to ‘1’ and performing a software store after tRTCp.
>The OSCEN bit in the calibration register at 0x1FFFF8 controls enabling and disabling of the oscillator. This bit is nonvolatile and is shipped to customers in the “enabled” (set to ‘0’) state.
>OSCEN must be set to ‘1’ by the user. This turns off the oscillator circuit
Thanks,
Shubham
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @NaMo_1534561 ,
>When you are not using the RTC functionality in an nvSRAM with RTC, the RTC-related pins of the part (XIN, XOUT, VRTCcap, and VRTCbat) must be left floating as already you have pointed out. Also, you must ensure that the RTC oscillator is disabled by setting the OSCEN bit to ‘1’ and performing a software store after tRTCp.
>The OSCEN bit in the calibration register at 0x1FFFF8 controls enabling and disabling of the oscillator. This bit is nonvolatile and is shipped to customers in the “enabled” (set to ‘0’) state.
>OSCEN must be set to ‘1’ by the user. This turns off the oscillator circuit
Thanks,
Shubham