Did you know that the serial nvSRAM RTC can be configured to detect half/quarter a second ?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MeduH_46
Employee
Employee
5 sign-ins 10 replies posted 5 replies posted

Hi All,

   

The new serial nvSRAM RTC devices can be used to detect less than a second using its newly added Square Wave generation feature. nvSRAM RTC devices can generate Square wave of  frequencies 1 Hz, 512 Hz, 4096 Hz and 32768 Hz on INT pin. This along with RTC time keeping registers can be used to count less than a second.

   

Regards,

   

Harsha

0 Likes
0 Replies