I am currently working on CY14C101J1 nvSRAM ,interfaced to atmega2560. I am facing issue related to retrieve the  data from nvsram after power off and on condition.

case: 1

int main()

{

    int8_t str[4] = {0xFF,0xBB,0xCC,0x55};

    int8_t rx_buffer[20];

    int8_t rx_buff[1];

   for(i=0;i<4;i++)

   {

         str = 0;

   }

    EEPROM_Memory_Write(&str,4,SLAVE_WRITE_ADDR1,0x1234);

    EEPROM_Commnd_Write(SLAVE_WRITE_ADDR1 , COMMND_REG, ASENB );

    EEPROM_Commnd_Write(SLAVE_WRITE_ADDR1 , COMMND_REG, STORE);

    EEPROM_Memory_Read(SLAVE_READ_ADDR1,SLAVE_WRITE_ADDR1,&rx_buffer,4,0x1234);

    _delay_ms(8000);

}

here, i am able to read the data in rx_buffer as 0xFF,0xBB,0xCC,0x55 before power off condition.

case: 2 But when i make the power off the board and power on ,i am not able to retrieve the same data in memory location (0x1234) .It showing some junk data . i tried the below steps to read the data.

    EEPROM_Commnd_Write(SLAVE_WRITE_ADDR1 , COMMND_REG, RECALL);

    _delay_ms(8000);

    EEPROM_Memory_Read(SLAVE_READ_ADDR1,SLAVE_WRITE_ADDR1,&rx_buffer,4,0x1234);

  

please help me to find the solution to read actual data after making  power off and on condition.For your reference,find below attached files.

*provide some pseudo code or steps to achieve?

Reply as soon as possible.

Thanks,

Arjun

0 Likes
1 Solution
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

We checked the schematics and found a external connection between VCC and the capacitor connected to the Vcap pin. Externally no connection was required. On removing the connection, the board is now working properly.

Thanks,

Pradipta.

View solution in original post

0 Likes
1 Reply
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi,

We checked the schematics and found a external connection between VCC and the capacitor connected to the Vcap pin. Externally no connection was required. On removing the connection, the board is now working properly.

Thanks,

Pradipta.

0 Likes