Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

Sort by:
Translation_Bot
Motor Control ICs
Hi, I am trying to send firmware, parameters and scripts to IMC101T using stm's uart. Now we just want to communicate something as simple as connectin... Show More
JaydenCai
Motor Control ICs
Main parameters and features:· Control method: non-inductive FOC · Current sampling: single resistor · Working voltage: 220V AC · Output power: 200W ... Show More
JaydenCai
Motor Control ICs
This solution uses the Infineon motion control chip IMM101T to drive the motor. Through precise control algorithms, the motor can reach a high speed o... Show More
AG_Serad
Motor Control ICs
I read the online documentation: AN2020-25 Handling multiple motor…. But I think there are a problem into the proposed VB script And/Or MCEWizard. Ple... Show More
DOUMBIA
Motor Control ICs

HI 

it is my file for configuration  for me it is correct and corresponding with datasheet TLE9180

Best Regards

DOUMBIA
Motor Control ICs
Hello, I work on motor driver TLE9180  i have any problem  I tried to read the status register of a Infineon IC(TLE9180D). MISO line,I don't receive a... Show More
User22801
Motor Control ICs
In general, it is recommended to connect unused WKx pins to GND.However, it is possible to leave the unused WKx pins floating, as long as the internal... Show More
User22801
Motor Control ICs
TLE9210x - What is the value of CSA1L field in a situation where Rshunt is in series with motor and motor changes rotation direction?1. In a situation... Show More
User22801
Motor Control ICs
The static charge current ICHGST and the static discharge current IDCHGST for static activation are used for two purposes:1. These currents are used t... Show More
User22801
Motor Control ICs
How to treat unused gate drivers when the static brake or the VS overvoltage brake are used for the TLE9210x product family?SHx must be connected to G... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.