Motor Control ICs Forum Discussions
I use M1_ IMC101t and M1_ IM241 official development board debugging motor, for the hardware part, I directly use Infineon official hardware.
The configuration parameters of the motor include resistance, ld, lq, KE, etc. I have confirmed multiple times with the motor factory that the parameters are correct.I use VF diagnosis to adjust vd_ Ext and speed can obtain stable waveforms.
However, when using the motor in practice, it was found that the current was very small and the motor was still unstable. I set the motor speed to 50RPM and adjusted issues 58, 60, 58, 64 kp, and 65 ki, but after trying for a long time, I was unable to obtain a FLX close to 2048_ M. How to make FLX_ Is M stable and like DC? How to make Flux_M be steady and DClike?
Show Less
Hello!
IMC102T datasheet states that it can controll totem-pole PFC.
Are there any examples of using TP PFC?
I can not find it in design software. Only reference is on IEEE article and
EVAL-M3-CM615TN, with no more information.
Best regards,
Karol
Show Less
Hi Infineon's friends:
Attached is the schematic diagram of our TLE9183. I would like to ask you to help review the following to see if there are any unreasonable points, thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/TLE9183-%E5%8E%9F%E7%90%86%E5%9B%BE%E5%AE%A1%E6%A0%B8/td-p/648183
Show LessI have implemented the Constant-power control for our PMSM motor for Fan Application using following application note
In our ongoing efforts to integrate the RF remote with the Motor Controller using Attiny85 as the interface controller, I have a query regarding the UART command for controlling TargetPower.
Now, I seek guidance on the appropriate UART command syntax and procedure for achieving TargetPower control.
Show Less
Dear Sir or Madam,
I got a TLE94112 HAT planned to Raspberry PI 4 B, But when I tried to install the multi-half-bridge library (https://github.com/Infineon/multi-half-bridge) by using "sudo pip install multi-half-bridge", I got some errors that it can NOT find the source files, the pybind11 version I installed in 2.11.1.
Can someone help me to fix this issue?
Thanks!
Albert
Show Less
can we use Segger J-Link Debugger for other than Infineon uC , family , if yes please share connection diagram,
Hi,
Input capacitor (DCLINK) calculation for single phase motor bridge (infineon.com)
I stumbled upon this application note, which is very well written and serves as a guide for sizing the DC link capacitor for a DC bus.
There is a phenomenon that I cannot seem to justify in my head, and after doing my own analysis I feel I lack some understanding of why it is happening.
Page 14 shows a graph where VSpp (ripple) increases with duty cycle as you would expect, but when it reaches 70%, the VSpp starts to roll off. After doing my own analysis based on my own parameters and the set up described in the application note, I get the same results. VSpp starts to decrease when it reaches this threshold of around 70%. The calculated values are backed up by the real-world measured values, which adds a lot of credibility to this application as a design resource.
Intuitively, I feel this has something to do with the interplay between D, (1-D), ESR and the energy balance between the DC LINK and the inductance of the motor. But I cannot quite put my finger on it, is there a name for this phenomenon? Why does it happen?
Thanks,
H
Show Less
Hello,
I wanted to understand which all types of hall sensors are compatible with the IMC301a IC. I am trying to use ABI encoders and I am wondering if it will be compatible with the IC.
Show Less
ISD平台下 选用IMC102T-64PIN 芯片开发的工程,跑长运时,驱动报CPU execution fault 故障后,不能发清除指令清除,必须给芯片断电后重新上电复位才能清除CPU execution fault 故障。
问题:1、 确定CPU execution fault 故障是不能通过清除故障指令清除吗?
2、该故障时跑长运实验时,运行8个小时以上后才报的,有什么好办法排除该故障吗
Show LessHello everyone. Recently, the IMC101T-T038 chip was used to control a permanent magnet synchronous motor, and an MCU was used to communicate with the IMC101T-T038 through the UART port. After several months of operation, it was discovered that the chip was unable to communicate. The on-site inspection revealed that the MCU had sent a message to IMC101T-T038. The IMC101T-T038 had no response. The oscilloscope was used to check the transmission and reception foot waveforms. The MCU had transmitted waveforms, and the IMC101T-T038 did not respond to the waveforms. Communication returns to normal after the power is turned on again. The firmware burned by IMC101T-T038 is IMC101T-T038_A_v1.03.03.ldf
I just discovered on Infineon's official website that the IMC101T-T038_v1.03.07_releaseNotes document has the following instructions. Please ask the experts to help me to see if this problem in the MC101T-T038_A_v1.03.03.ldf firmware is causing the IMC101T-T038 to fail to communicate with the MCU. Thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/IMC101T-T038-uart-%E4%B8%8E%E4%B8%BB%E6%8E%A7%E9%80%9A%E8%AE%AF%E6%95%85%E9%9A%9C/td-p/641687
Show Less