Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

Sort by:
Translation_Bot
Motor Control ICs
Hello everyone. Recently, the IMC101T-T038 chip was used to control a permanent magnet synchronous motor, and an MCU was used to communicate with the ... Show More
Kaleeswaran
Motor Control ICs
hello all,        how to measure hall angle offset in mce wizard.  I am using 3 digital hall sensors, each displacement by a 120-degree electrical ang... Show More
wang1
Motor Control ICs
请教一个问题:我在使用串口通信时,配置模式是FIFO,然后配置接收字节是12个字节,正常通信时字节数是12个,通信正常。但是当通信过程中有异常时,字节数会多于12个或小于12个,这时会导致串口无法接收数据,然后当字节数恢复为12个字节时,单片机还是接收不到数据。感觉像是串口卡死了一样,无法恢复,请问... Show More
GrCa_1363456
Motor Control ICs
What guidance is available for Stepper Motor Drive? Infineon has one active Stepper Motor driver, TLE8444SL with 4 channels rated to 0.8A and 18Volts.... Show More
yb841123
Motor Control ICs

请问大家TLE9180的demo在哪里可以下载?谢谢

Kaleeswaran
Motor Control ICs
hello all,  normally I start the motor in Mce Designer It works, but when I tried to use the “VF Diagnostic” function on the motor1 page it showed a g... Show More
JasonLEE
Motor Control ICs

Can you tell me what the clock frequency is for this module?

Please reply.
Thank you.

wang1
Motor Control ICs
我使用ISD调试开环电压控制模式,我将Vq_Ext设置为18%,转速设定为220rpm,额定电流设置为4A,直流母线电压为380V。 通过示波器观察相电流有效值为6A,请问这是怎么回事呢?另外,使用开环电压控制模式,功率模块发热非常严重,直接让功率模块烧坏了,请问这个应该怎么去调试呢?我尝试过缓慢增... Show More
wang1
Motor Control ICs

请教一下,电机在堵转时我检测motorspeed和AbsMotorSpeed值,发现这两个值都是有值的。那么现在这个问题会导致我无法判断电机是否正常启动,请问有没有其他的办法可以检测电机是否启动正常呢?

bert1268
Motor Control ICs
电机参数为 Lq=12.7mh,Ld=8.9mh,Rs=0.86欧, 电流环设置带宽为120rad/s, 速度环参数设置为kxSreg=0.00067  KpSreg=8  SpdFiltBW=0.02, 电流采样配置为  SHDelay = 0.396us   TMinPhaseShift = 3... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.