Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

User22801
Motor Control ICs
In general, it is recommended to connect unused WKx pins to GND.However, it is possible to leave the unused WKx pins floating, as long as the internal... Show More
User22801
Motor Control ICs
TLE9210x - What is the value of CSA1L field in a situation where Rshunt is in series with motor and motor changes rotation direction?1. In a situation... Show More
User22801
Motor Control ICs
The static charge current ICHGST and the static discharge current IDCHGST for static activation are used for two purposes:1. These currents are used t... Show More
User22801
Motor Control ICs
How to treat unused gate drivers when the static brake or the VS overvoltage brake are used for the TLE9210x product family?SHx must be connected to G... Show More
User22801
Motor Control ICs
There is no risk in driving VDD and EN pin together from a single microcontroller I/O pin, since when EN =0 device is in Sleep mode and there is no ac... Show More
User22801
Motor Control ICs
Rotation from HS1 to LS2:1. SPI FRAME: 0b 1100 1101 0000 0000 0000 0110– HB1MODE = 10b HS1 ON– HB2MODE = 01b LS2 ON2. SPI FRAME: 0b 1100 1111 0000 000... Show More
User22801
Motor Control ICs
Are the charge pumps of the TLE92104 and TLE92108 still working in the case of fault condition?In case of a fault on a half-bridge driven by the devic... Show More
User22801
Motor Control ICs
Is it possible to independently drive HS and LS stages of a single half-bridge for the TLE9210x?The HSx and LSx outputs of a single half-bridge cannot... Show More
User22801
Motor Control ICs
Here is the recommendation from Infineon.Place the filter (both resistor and capacitor) close to the shunt resistor• Therefore the eventual noise is f... Show More
User22801
Motor Control ICs
Why is the power-on reset bit of the global status byte active low at the TLE92104 and TLE92108?Unlike the other status bits of the global status byte... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.