Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

Translation_Bot
Motor Control ICs
For the application scenario of driving a three-phase motor, does the TLE9180D32QKXUMA1 chip support the active short Cut (ASC) function?smartconx_tar... Show More
Mahimc2020
Motor Control ICs
Thank for your precise and fast response"PFC Control Registers in iSD Script Editor ". for the second question: I wrote "GPIO21 == 0" in MCEWizard and... Show More
Mahimc2020
Motor Control ICs
Hi i used MCE Wizard (script coding) before and the PFC registers, for example PFC_ACPOWER. Now im using iSD and i want to transfer the old script to ... Show More
alex-d
Motor Control ICs
Hello, I understand that the iMotion product line includes the iMotion link, which allows users to program and debug boards for development purposes. ... Show More
wph1995
Motor Control ICs
Hello, I am designing a circuit to control a brushless motor of 311VDC / 2A @ 15000rpm. I have decided to use the IMC302A-F064  controller, currently ... Show More
bert1268
Motor Control ICs

IMC102T-64pin 芯片的41脚功能是LED,这个LED灯有哪些显示状态, 分别表达什么含义

Xuehs
Motor Control ICs
我想使用这个评估版,于是我看了EVAL_IMD700A_FOC_3SH 18 V brushless DC motor drive board,但是有点疑惑,如下两个图片 第一个图片是在文档的第49页,表格里显示RS1、RS2、RS3三个采样电阻阻值为100毫欧,但是第二张图片的原理图里又显示他... Show More
Kaleeswaran
Motor Control ICs
Hi everyone,       kindly clarify my doubts in imc101t-f048 controller. 1) Based on the current sensing range single shunt and leg shunt will differ? ... Show More
QiaoxiLiu
Motor Control ICs
  i want to change motor rampup speed,as the picture bellow,PMSM_FOC_INPUT.ref_speed  rampup time is 110ms but the PMSM_FOC_OUTPUT.rotor_speed can not... Show More
Translation_Bot
Motor Control ICs
Hi, I am trying to run a combination HybridKit Drive and Axial Flux machine. While making settings in One eye, I came across the part where I set the ... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.