Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

seb_44120
Motor Control ICs
Hello, We bought the EVAL-M1-101TF + EVAL-M1-05F804R Combo and tried to spin a standard Brushless Motor. Motor used is : QBL4208-41-04-006   Specifica... Show More
yangyong
Motor Control ICs

Excuse me, is 96mhz an on-chip crystal oscillator or a CPU frequency?  Is it output by PLL?

MathanRaja
Motor Control ICs
Hi, I am using Eval IMM101T-046M. Initially, I can connect the board to MCE Designer and can program using MCE Designer. But now I can connect the boa... Show More
User20393
Motor Control ICs
Hi My IMC101 is working well with UART Control Interface. However after using script of UART_DriverInit(1 /*channel*/, 0 /*rxInvert*/, 0 /*txInvert*/,... Show More
cw2611
Motor Control ICs
I am designing a BLDC controller using IMC302AF064XUMA1 controller. I will be configuring the controller using the iMotion link software wizard. From ... Show More
seb_44120
Motor Control ICs
I just tried to register my product, but the EVAL-M7-D111T is not in the list (see attached picture). Is there another place to fin the configuration ... Show More
User20393
Motor Control ICs
Hi In constant power control Yes i can calculate the power by using script, Thanks to Appnote AN2020 Is it possible to send target power thru UART1 wr... Show More
yarzar
Motor Control ICs
Does IMC300 support CMSIS RTOS2 on Keil? After I include CMSIS RTOS library into the project, I can build successfully with compiler v6. When I try to... Show More
shirazmacuff
Motor Control ICs
Figure 8 in the IMC301 software manual shows leg shunts (low side of the bridge) for phases A,B and C. Does the control algorithm support in-line curr... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.