Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

sohail
Motor Control ICs
Hi @Krupashankar               Someone Pl Guide how to Get Variables Data in MCE Designer. As per doc 2.6.5 Variable types and scopeScript engine supp... Show More
cw2611
Motor Control ICs
Hey! I want to run a 36V BLDC motor with peak current at 11A. Do you have any evaluation board that contains both the microcontroller as well as the h... Show More
sohail
Motor Control ICs
Hi,             I write my own  script code in MCE Designer, after compiling it shows the file script Function compile Complete. but this file is not ... Show More
NXTY_hayashi
Motor Control ICs
Hi, I can find nothing on Infineon web site about EVAL-M1-1302. If you have the schematics of EVAL-M1-1302 board, please send me it.   Best Regards, K... Show More
sohail
Motor Control ICs
Hi,        I am using EVAL-M3-302F I want to run simple program Blink led. I tried compile but there is error in IMC300A.h header file & imc300a_port1... Show More
cw2611
Motor Control ICs
Hello  I am trying to configure the BLDC motor using the MCE wizard, can the motor directly be operated using the MCE wizard? or do we need the SPI or... Show More
SBitney
Motor Control ICs
Hi,I'm having issues reaching higher currents when loading down a motor driven by a IMC101. I've got a maximum current limit of 3.5A set, and it will ... Show More
sohail
Motor Control ICs
iMOTION2go
solved msg Solved
Hi,           i just got motoin2go board, install MCEDesigner but when i open file IMC101T_V1.02.20_iMOTION2go.irc it give error product mismatch.  i ... Show More
User22801
Motor Control ICs
Regarding the VS quiescent of product TLE92104 and TLE92108, current during VS=13.5V and VDD=0V, is it still 2uA typ and 5uA max?Yes, the VS quiescent... Show More
User22801
Motor Control ICs
Infineon recommends to set the static charge / discharge current for the total turn-on / turn-off time to 600 ns to 1 µs.--> e.g. Ichg static = Qg(tot... Show More