Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

ChrisLec
Motor Control ICs
Hi everyone, For an embedded application with motor control, we need to drive either a BLDC 24V  or a 3-phase ACIM 230V or  brushed DC 24V. Obviously ... Show More
nambip
Motor Control ICs
The DC bus voltage scaling resistor in the EVAL-M1-IM818-A has 5000K (Five 1M in series)  , on the MADK IMC101T-T038 we have 13.2K. These configs have... Show More
aneedles
Motor Control ICs
I have been reading iMotion 2.0 Device Programming document and trying to understand the whole process of taking a txt file generated by MCE Wizard (s... Show More
aneedles
Motor Control ICs
I have been reading iMotion 2.0 Device Programming document and trying to understand the whole process of taking a txt file generated by MCE Wizard (s... Show More
Beautr
Motor Control ICs
Hi, everyone: I would like to know how I format the data to be sent when the microcontroller uses SPI and TLE9562-3QX communication. For example, when... Show More
davisonInfineon
Motor Control ICs
I am attempting to read some of my script registers through the user UART interface (UART1). I am using the address given to me by the MCEWizard compi... Show More
Esra
Motor Control ICs
Hi, I want to drive two motor by four  half bridge driver circuit controlled by TLE92104. I followed this parts for HB1: 1-I configurated to BDPASS=0.... Show More
Gin
Motor Control ICs
Hi   I'm using TLE9562-3QX to control a DC motor to rotate clockwise, stop and brake then rotate counterclockwise. I set both HB1 and HB2 to LS_ON,  A... Show More
davisonInfineon
Motor Control ICs
I am having a problem with viewing scaled current on the IMC101TT038XUMA1. I have the parameters set to use Leg Shunt, and have current sensing gain a... Show More
张晨
Motor Control ICs
TLE7182EM
solved msg Solved
When TLE7182EM chip is in use, the input IH1 is set to high level, then why does the GH1 output have 10V voltage? According to the specification, this... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.