Motor Control ICs Forum Discussions
Sort by:
Motor Control ICs
Hello all,We are trying to evaluate the EVAL-M1-101T evaluation board based on IMC101T-T038.We are using MCEWizard for configuring motor parameters an...
Show More
Hello all,
We are trying to evaluate the EVAL-M1-101T evaluation board based on IMC101T-T038.
We are using MCEWizard for configuring motor parameters and using MCEDesigner to program the IC.
We can program all the files as suggested in the user manual in the following link.
https://www.infineon.com/dgdl/Infineon-An2018-01_EVAL-M1-101T_User_Manual-UM-v01_06-EN.pdf?fileId=5546d462625a528f01629491d86c39ba
Our application requires driving an induction motor, and thus we are following the Infineon application note for getting our motor run.
https://www.infineon.com/dgdl/Infineon-Induction_motor_control_by_iMOTION-ApplicationNotes-v01_00-EN.pdf?fileId=5546d4626cb27db2016d011d354c0032
I have successfully configured and programmed the IC according to the document. But when I upload the script, I get version mismatch in the MCE Designer.
As we look forward to manufacturing at least 1000 numbers of the VFD using this IC per month, but can't find the problem.
I have attached the error image for reference.
Any help would be highly appreciated.
Thanking you in anticipation.
Show Less
We are trying to evaluate the EVAL-M1-101T evaluation board based on IMC101T-T038.
We are using MCEWizard for configuring motor parameters and using MCEDesigner to program the IC.
We can program all the files as suggested in the user manual in the following link.
https://www.infineon.com/dgdl/Infineon-An2018-01_EVAL-M1-101T_User_Manual-UM-v01_06-EN.pdf?fileId=5546d462625a528f01629491d86c39ba
Our application requires driving an induction motor, and thus we are following the Infineon application note for getting our motor run.
https://www.infineon.com/dgdl/Infineon-Induction_motor_control_by_iMOTION-ApplicationNotes-v01_00-EN.pdf?fileId=5546d4626cb27db2016d011d354c0032
I have successfully configured and programmed the IC according to the document. But when I upload the script, I get version mismatch in the MCE Designer.
As we look forward to manufacturing at least 1000 numbers of the VFD using this IC per month, but can't find the problem.
I have attached the error image for reference.
Any help would be highly appreciated.
Thanking you in anticipation.
Motor Control ICs
Hello Everyone, I want to interface IC IMC101T-T038 with Arduino Uno. How can I use interface pins of IMC101T-T038 with Arduino Uno? ( iMOTIO...
Show More
Hello Everyone,
I want to interface IC IMC101T-T038 with Arduino Uno. How can I use interface pins of IMC101T-T038 with Arduino Uno?
( iMOTION™ motor controller IC IMC101T-T038 have interface pins but no description available in the datasheet ) Show Less
I want to interface IC IMC101T-T038 with Arduino Uno. How can I use interface pins of IMC101T-T038 with Arduino Uno?
( iMOTION™ motor controller IC IMC101T-T038 have interface pins but no description available in the datasheet ) Show Less
Motor Control ICs
Hi , I intend to use 2 BTN 8982TA on a H bridge to control a DC motor. But I want to recover energy from the DC motor coupled with an inductor and se...
Show More
Hi , I intend to use 2 BTN 8982TA on a H bridge to control a DC motor. But I want to recover energy from the DC motor coupled with an inductor and send it back to the battery to charge it when the motor is in generator mode. My first question is: May I use the 2 controls pin per half bridge to generate the appropriate sequence to have the bridge in boost mode.? please give me details.
Show Less
Motor Control ICs
"I have set up a working bi directional motor from this H bridge and would like to read the current being drawn by the motor. I am trying to output th...
Show More
"I have set up a working bi directional motor from this H bridge and would like to read the current being drawn by the motor. I am trying to output the current from the IS_1 / IS_2 analogue output pins to my Arduino uno but i cannot get it to work. I do not know what the correct procedure is. if i simply analogRead(0) i get a constant value. How are you supposed to do this??
ps. i have hooked up an ammeter so i know the system works well " Show Less
ps. i have hooked up an ammeter so i know the system works well " Show Less
Motor Control ICs
"I would like to ask about using BTN8962TA supported with stm32f103cb to produce PWM signal for 50W load.My question is .. what kind of software libr...
Show More
"I would like to ask about using BTN8962TA supported with stm32f103cb to produce PWM signal for 50W load.
My question is .. what kind of software library can I use for this half-bridge.
IN-INH-IS pins is giong to the stm microcontroller whereas ""IN"" pin is enough to transfer the PWM signal from the stm to the chip." Show Less
My question is .. what kind of software library can I use for this half-bridge.
IN-INH-IS pins is giong to the stm microcontroller whereas ""IN"" pin is enough to transfer the PWM signal from the stm to the chip." Show Less
Motor Control ICs
There seem to bee two different specifications for the INH and IN pins. In the first part of the document there are max ratings of 5.3 volts (See sect...
Show More
There seem to bee two different specifications for the INH and IN pins. In the first part of the document there are max ratings of 5.3 volts (See section 4.1.4 in datasheet), and 2 volts in section 5.4.1. Would it be okay to operate these pins at 3.3 volts
Show Less
Motor Control ICs
In the product data sheet, please refer to ""Figure 16"". Let's assume two changes in my application:1 - My power supply will be a 35V battery power ...
Show More
In the product data sheet, please refer to ""Figure 16"". Let's assume two changes in my application:
1 - My power supply will be a 35V battery power supply
2 - The motor ""M"" will be replaced by a highly inductive load (essentially a coil) that is about 500mH and a DC resistance of 2.9 ohms
Questions:
With a highly inductive load replacing ""M"", it would cause voltage surges back to the power supply, how can the supply be protected?
What is the effect of the flyback current from the inductive load on the battery supply?
What precautions should I take to protect it? The most obvious seems to be the use of a diode from the battery in series to the circuit.
" Show Less
1 - My power supply will be a 35V battery power supply
2 - The motor ""M"" will be replaced by a highly inductive load (essentially a coil) that is about 500mH and a DC resistance of 2.9 ohms
Questions:
With a highly inductive load replacing ""M"", it would cause voltage surges back to the power supply, how can the supply be protected?
What is the effect of the flyback current from the inductive load on the battery supply?
What precautions should I take to protect it? The most obvious seems to be the use of a diode from the battery in series to the circuit.
" Show Less
Motor Control ICs
For the moment I am using VN771KE from ST. Does BTM7750G/BTM7740G match the ST device? If not, could please recommend a device which can replace VN771...
Show More
For the moment I am using VN771KE from ST. Does BTM7750G/BTM7740G match the ST device? If not, could please recommend a device which can replace VN771KE? Thanks
Show Less
Motor Control ICs
I am informed that BTM7740G/BTS7740G will be discontinued and not recommended for new design. Could you please recommend the device for replacement?Th...
Show More
I am informed that BTM7740G/BTS7740G will be discontinued and not recommended for new design. Could you please recommend the device for replacement?
Thanks Show Less
Thanks Show Less
Motor Control ICs
I would like to use BTN8962TA for a 24V application. The peak voltage might reach 30V. I noticed the max. normal operating voltage range of VS is 18V ...
Show More
I would like to use BTN8962TA for a 24V application. The peak voltage might reach 30V. I noticed the max. normal operating voltage range of VS is 18V and the extended operating voltage range is up to 40V.
Could you please explain the affects if I use the device for 24V application? Show Less
Could you please explain the affects if I use the device for 24V application? Show Less