Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

Polar
Motor Control ICs
Dear all, I would like to ask you wether I can use the component TLE7209-3Raum instead of TLE7209-2R ? I had a look at tbe specifications and the only... Show More
kkkkjeong
Motor Control ICs
Hi, I'm going to run the motor using the imotion solution.   i  operated motor without pfc. but i can't operate pfc. how to clear faults like photo?th... Show More
kevinhaddaway
Motor Control ICs
hi  can anyone advise me of  the cause of a problem that I have. I have built a PCB  that is a copy of the evaluation  pcb schematic.  It is being con... Show More
Abc1
Motor Control ICs
  I have exactly the same problem as already described in this link. It says that it has been solved. As I understand it I have not solved the problem... Show More
Abc1
Motor Control ICs
Hi, how can I activate the field for the Class B safety ? for me it is grayed out. I use the IMC102 T64     thx Show More
yangyong
Motor Control ICs
motor parameters: 220vac,maximum power:1.2kw rated Amps: 10A Poles:  10 Stator resistance:  3.15ohms Lq  inductance: 0.93mH Ld inductance:0.93mH Back ... Show More
seb_44120
Motor Control ICs
Hi, this is the following post of  EVAL-M1-101TF configuration. We changed our parameters as described in your replies, and test some other different ... Show More
Vel
Motor Control ICs
Hi,   I am using I motion solution designer to tune my motor controller (IMD111T). I can see some fault has triggered and the motor stopped. Have no i... Show More
MathanRaja
Motor Control ICs

Hi,

I am using IMM101T-046M IPM.

If the pump got seizes, How is it will Handle it?

Thanks

Mathan

DevendraKumar
Motor Control ICs
Hi Team, I need some information related to MCE designer. Can you help me How to see V/F ratio in MCE Designer tool?   Thanks & Regards Devendra   Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.