Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

bert1268
Motor Control ICs
选用方案:压缩机电流单电阻采样,采样电阻阻值为5毫欧,采样电路中的上来电阻是7500欧,下拉电阻是330欧, 问题:使用ISD搭建的工程,配置好参数,烧录进芯片,通过模拟示波器查看Iu,Iv,Iw的值,在实际电机电流为0的情况下,在模拟示波器上看到电流值都会出现最大3A以上的突变,如附图所示(图中的... Show More
PaulojM
Motor Control ICs
Hi everyone, I want to show the motor voltage to the users, and for that i will use the MotorVoltage register. I am having a bit of problem with the c... Show More
PaulojM
Motor Control ICs
Hi everyone, I want to check if the input current when the PFC is ON normally has this spikes. The spikes appear when there is no motor running, they ... Show More
VolNK
Motor Control ICs
Hello Community, we have replaced a BTN8960 by a BTN8962 because the BTN8960 was discontinued. Unfortunally I do not have an old revision of the datas... Show More
Translation_Bot
Motor Control ICs
Hi Infineon. We had designed Ecu Based on TLE987. Now we need bootloader for reprogramming. But to Develop a new bootloader start form zero is ... Show More
Mac_Kurosawa
Motor Control ICs
In the "TLE6208-3G" Application Note, Rev. 1.0, July 2004, on page 20, in the description of the "Status Word" section, regarding "Bit 0: Overtemperat... Show More
Mahimc2020
Motor Control ICs
Hi, In previous version (MCE Designer) we could combine script file and parameter file and firmware file . Can we combine "out.ldf" and other "IMC102_... Show More
oscarkeser01
Motor Control ICs

Hi, 

Do we have a motor control plus PFC solution in a single microcontroller?

 

Thanks,

 

oscarkeser01
Motor Control ICs
Customer had a problem with EVAL M1 301F using Version 6.21 arm compiler. The below picture shows the L6236E error from an example project from Infine... Show More
Kaleeswaran
Motor Control ICs
Hello all we tried the imc101t-f048 controller for driving the BLDC motor(achieving 3000rpm in 2 seconds), but we could not achieve this using both th... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.