Motor Control ICs Forum Discussions
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/%E5%BA%94%E7%94%A8MCU%E5%AF%B9IMC102T%E5%92%8CIMC301A%E7%9A%84%E7%BC%96%E7%A8%8B%E9%97%AE%E9%A2%98/td-p/497033
Show Less1、The schematic diagram of the evaluation board downloaded from the website is completely inconsistent with the evaluation board, as shown below, please send a schematic diagram consistent with the evaluation board.
2、Please give the parameters of the evaluation board switching power supply output, the size of 15V and 3.3V output current.
3.Please give the parametric design method of auxiliary switching power supply, especially the calculation of switching transformer.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/EAL-M1-IM818-A%E8%AF%84%E4%BC%B0%E6%9D%BF%E4%BD%BF%E7%94%A8/td-p/492195
Show LessOnce iMOTION ™ Solution Designer ( Version: 1.1.1.202303151810 ) is installed, open iMOTION ™ Solution Designer does not install the package after clicking Package Manager.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/iMOTION-Solution-Designer%E5%AE%89%E8%A3%85%E9%97%AE%E9%A2%98/td-p/489350
Show LessHi all,
So I have the EVAL-M3-IM564 motor driver module with the EVAL-M3-302F controller module.
I set up everything like it's mentioned in the datasheets. Except for a few parameters for the PFC part, I didn't know what to enter. Specificly Kp and Ki for the voltage and current amplifier. I used the standard values but I kept running into DC overvoltage fault. So I thought it had to do with the PFC settings, after changing them a few times, I kept having the same fault.
So I changed them up some more and wanted to start the PFC, and then the RS3 of the power board module blew up.
I did start PFC before the motor was running, I don't know if that was the cause?
Could anyone help me figure out how to calculate the correct values... Any help is appriciated!
Mike
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/EAL-M1-IM818-A%E8%AF%84%E4%BC%B0%E6%9D%BF%E4%BD%BF%E7%94%A8/td-p/485646
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/EAL-M1-IM818-A%E8%AF%84%E4%BC%B0%E6%9D%BF%E4%BD%BF%E7%94%A8/td-p/486552
Show LessI want to use an Arduino board to drive a 12V DC motor with a no-load current of 0.18A, a blocking voltage of 4A, and a maximum power of 4.34W. Originally, I chose the L293, but then I was confused about the choice of the H-bridge control chip because I considered a conveyor, which would probably be blocked in actual use.
Should I choose a chip with a maximum current of more than 4A?
I hope engineers can help answer the question about how to choose a DC motor driver chip, and explain whether to choose a chip with a maximum current over 4A. Thanks~😀
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/%E5%85%B3%E4%BA%8E%E7%9B%B4%E6%B5%81%E7%94%B5%E6%9C%BA%E9%A9%B1%E5%8A%A8%E8%8A%AF%E7%89%87%E7%9A%84%E9%80%89%E6%8B%A9/td-p/481657
Show LessI have recently used ISD imotion for configuring hardware and software, and now I have "generated" folder which contains parameter setting information and the output file for programming.
There are two *.ldf files in this folder. A *.ldf file whose name starts with a device name (in this case, IMC102TF064) is an image of the firmware for the device. Another *.ldf file named "out.ldf" contains parameter and script images.
Now I want to know if I could Program my MCE by FlashPro – iMOTION (X2S) relates from Elprotronic company or not?
Show LessCan you tell me if there is any documentation on the IMD111/112 which are with pre-drive, what is the maximum current that can be driven and what is the maximum power that can be driven to the motor?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/IMD111-112%E5%8F%AF%E4%BB%A5%E6%94%AF%E6%8C%81%E7%9A%84%E6%9C%80%E5%A4%A7%E5%8A%9F%E7%8E%87/td-p/478275
Show Less