Motor Control ICs Forum Discussions
Hi Sir/Madam,
I would like to confirm is the Pin of 39 & 40 of IMM101T-046M, is that necessary to mount on PCB Board ?
I had check the PCB Layout of EVAL-IMM101T ( iMOTION™ MADK Starter Kit for IMM101T Smart IPMs),
--> there is no solder pad on it.
But information in Datasheet, Note is mentioned :
--> " Pins 39 and 40 are not required to be connected electrically on the PCB but are recommended to be soldered for mechanical stability. "
Does it means the pad need or need not to solder on board ?
Pls advise. Thanks.
Show LessHi Sir/Madam,
I would like to confirm is the Pin of 39 & 40 of IMM101T-046M, is that necessary to mount on PCB Board ?
I had check the PCB Layout of EVAL-IMM101T ( iMOTION™ MADK Starter Kit for IMM101T Smart IPMs),
--> there is no solder pad on it.
But information in Datasheet, Note is mentioned :
--> " Pins 39 and 40 are not required to be connected electrically on the PCB but are recommended to be soldered for mechanical stability. "
Does it means the pad need or need not to solder on board ?
Pls advise. Thanks.
Show LessHi i am using EVAL M3 IM564 and EVAL M3 102T.
QUESTION 1
I want to run using UART.
So, first i send a message to MCE
(01 06 01 20 00 00 FE D9)
And i sent a message to operate at 3000rpm
like below.
01 03 00 00 b8 0b 47 f1
But operation is different that using ISD.
ISD is good condition.(3000rpm)
UART is working and then it stops.(2000rpm->stop)
why is it that?
QUESTION 2
Where are parameter lists?
I can't find it.
Thank you at all times.
Show Less
We found different LOT numbers in the same reel. Is this normal?
Hi i used EVAL-iMOTION2go.
I changed User/Host COMM port selection (UART1->0)
And download firmware.
At that time the connection is not.
1. how to reset that?
2. is firmware download program is only one?(iMOTION Solution Designer)
Show Less
Hi,
I'm planning to buy EVAL-M3-IM564 but I need some information regarding PFC circuitry.
I want to know from where PWM signal for PFC control is generated. Whether it's from configuration board IM564 or from some controller present on EVAL M-102T ?
Regards,
AsadBashir160
Show LessMCE supports totem-Pole PFC topologies. But all development boards are boost PFC topologies. Can you provide the reference circuit of totem-Pole PFC topologies。
thanks!
Show LessHi Sir,
I had just bought an EVAL-IMM101T-046TOBO1 Brd for testing BLDC Motor.
I set the Parameter in MCEWizard and program into EVAL brd by apply MCEDesigner.
Once program successfully, I press the button of "Configure Motor" and press the button of "Start Motor" as below :
But once I press the "Start Button" , suddenly the Board burn immediately.
What is causing the board burned ? The Parameter shouldn't cause the board burn for the testing.
Pls advise.
EVAL-IMM101T User Manual (infineon.com)
Show LessDear all,
I would like to ask you wether I can use the component TLE7209-3Raum instead of TLE7209-2R ? I had a look at tbe specifications and the only difference seems to be that 3R has a larger output current than the 2R. (These IC's are used to control qas ventitile in benzin cars, like, for example, Peugeot 206).
Thank you for your help,
Polar
Show Less
Hi, I'm going to run the motor using the imotion solution.
i operated motor without pfc.
but i can't operate pfc.
how to clear faults like photo?
the faults occur always.
please advise for me
Show Less