Motor Control ICs Forum Discussions
hey,friends.
now i am working with tle9183qk to drive the three-phase motor. And please see the attached picture below.Where is the supply voltage of the current sense amplifier provided, is it artificially adjustable, I want to artificially create this fault to verify the mechanism in the picture.Can you give me some suggestions, such as whether it is possible to change some power supply voltage to create the fault
Show LessHi
I am using the M7-D111T Eval-Board with the M7-LVMOS-INV Powerstage. Im still at the beginning of getting my motor to run, however i'm stuck at connecting the Eval-Board with the iMotion Solution Designer.
The Board ist powered with 24VDC, i checked the Voltage Levels of the 5V and the 12V output, both are correct. (Picture of my Setup is attached). I am using the latest version of the iSD with the latest SD-Pack.
When clicking "Target->Connect" and using the right COM-Port (JLink CDC UART Port), the iSD is trying to connect to my Eval-Board. Also, the blue LED on the Eval-board ligths up. However, in the bottom left corner of iSD it says "target not connected". (check Screenshot of the Log file down below)
When using the Programmer, the output says "iMotion controller did not respond". Somehow, after trying to connect with the programmer several times, I got a connection with the warning "The connected device does not match the device configuration". What does this mean??
Can someone help me with these errors?
Best regards
Show LessFor TLE9180-32QK, if there is a input current signal at pin61 and 62, then when could we get the output signal at pin 60? Actually, I just want to know the delay time.
There is an output settling time as step response in datasheet, could me use this parameter as delay time?
Show Less
Hi,
1. I installed the new Package V5.01.18 and now I can't enter more than 100A Inverter current. (I need 300A)
2. I can't enter Motor rated amps per phase more than 100A. (I need about 300A)
3. My current sense resistor value is 0.25 mohm (250 micro ohms). I can't enter such a value. (lowest value entry 0.1 mohms)
Please advise.
Show Less
Excuse me, a txt file was generated in the MCE 2.0 version, and you can see the conversion values of some variables. So in iMotion 5.0, how to see these values? Please see my picture.
Show Less
Hi,
I Started First Project in Imotion solution Designer. I am Getting Error when Run Motor.
1.Gatekill & GKPin.
I am using REF-AIRCON-C302A-IM564 Board.
Thanks
Show Less
Excuse me, the routine I open with imotion, there are 2 scripting languages in the script? Why is it written this way? Since I can only write one script with iMotion 2.0 before, please tell me that there are 2 scripts in the new version of Motion, and how can I use them?
Show LessHi,
i am Receiving Fault Flag Error no 65.Can someone Explain as in iMOTION™ Motion Control Engine
Software Reference Manual no Explanation.
Thanks
Show Less