Motor Control ICs Forum Discussions
text.format{('custom.tabs.no.results')}
Hi
Im looking at the example projects for IMC 301 F064, ADC example is giving me the error.
************************
No Algorithm found for: 00008000H - 00008A0FH
No Algorithm found for: 2000000CH - 2000014FH
Programming skipped!
Error: Flash Download failed - "Cortex-M0"
Flash Load finished at 13:09:17
*******************
I have the right algorithms as they were verified by CCUTimer example, could anyone throw some light on this concern?
Show LessHello! May I ask if there is any graphical programming software available for the TLE9562-3QX chip? Because I want the CPU to communicate with the TLE9562-3QX chip through SPI to control the motor operation, but I don't know how to write the initialization TLE9562-3QX code and driver code! So I would like to ask if you can tell me how to quickly write TLE9562-3QX initialization and driver code? Thank you!
Show LessHi @SarkarSushru @SarkarSushru
Thanks for reply "how to program imc102T-F064 with FlashPro – iMOTION (X2S) relates from Elprotronic company "
I used iMOTION_SD_V5.03.07.sdpack
This programmer is (FlashPro–iMOTION(X2S)) compatible with SD_V5.03.07.sdpack ?
Show Less
如题,我是用EVAL_IMD700A_FOC_3_Shunt和BPA软件调试电机,但是电机负载稍微大一点就会失步,电流大不起来,我该调整那些参数呢?
I want to use an Arduino board to drive a 12V DC motor with a no-load current of 0.18A, a blocking voltage of 4A, and a maximum power of 4.34W. Originally, I chose the L293, but then I was confused about the choice of the H-bridge control chip because I considered a conveyor, which would probably be blocked in actual use.
Should I choose a chip with a maximum current of more than 4A?
I hope engineers can help answer the question about how to choose a DC motor driver chip, and explain whether to choose a chip with a maximum current over 4A. Thanks~😀
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%9C%BA%E6%8E%A7%E5%88%B6%E8%8A%AF%E7%89%87/%E5%85%B3%E4%BA%8E%E7%9B%B4%E6%B5%81%E7%94%B5%E6%9C%BA%E9%A9%B1%E5%8A%A8%E8%8A%AF%E7%89%87%E7%9A%84%E9%80%89%E6%8B%A9/td-p/481657
Show LessHi
I'm using IMC101.
Motor Max RPM (MCEWizard) is 3,500 rpm.
In run time, the TargetSpeed is 16,383.
It turn out that the measured speed is 3,550 rpm.
Be confident 100% that my speed measurement is correct.
I have no idea to fix it.
pls help
Show Less
Good morning all, on the REFAIRCONC302AIM564TOBO1, some outputs are use for the LED status and one to shorcut the current limitation CTP trough a dry contact relay, I used the same pin number from F064 to the F048 and flash my custom PCA.
I can run the motor but never the LED and relay output change the state, my question where is this part of the firmware to order the relay and LEDs ?.
P0.10 -> Relay for startup current limitation
P0.08->Green LED
P0.13->Red LED
In advance thanks a lot for your support
Show Less