Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

ccitxue
Motor Control ICs

EVAL-M3- CM615PN评估板PFC电感要求大于3mH,请问这个3mH电感是如何计算出来的,并给出相应的计算公式。该评估板输出功率为650W,输入电压范围为176VAC-260VAC。

MathanRaja
Motor Control ICs
Hi, I am using an IMM101T-046M with STM32F303CBTx. I am controlling the two motors. for ex: I have stored the parameter file as follows in the IPM chi... Show More
LucasHall
Motor Control ICs
I am using the EVAL-M1-IM828-A and EVAL-M1-101T to prototype a BLDC motor application. "MCEWizard Configuration Files v1.0" from the iMOTION™ Modular ... Show More
PaulojM
Motor Control ICs
Hello, I have been trying to stop a motor using regenerative mode but i must be missing something because it is not working well.   MOTOR P = 750W 3 p... Show More
Translation_Bot
Motor Control ICs
Hi, I am trying to send firmware, parameters and scripts to IMC101T using stm's uart. Now we just want to communicate something as simple as connectin... Show More
Swap26
Motor Control ICs
Hello,I am writing a script which can dynamically change the motor current limit. I was going through the iMotion Software reference manual to underst... Show More
PaulojM
Motor Control ICs
Hi, I want to reverse a industrial door when someone is under it. To do that i tried to do the following steps inside the script: 1- Stop the motor, u... Show More
sahayacharles
Motor Control ICs
I can't able to communicate with IMC101T-F048 IC.  This is the second IMC101T-F048 IC I have changed. While first-time programming(Firmware & paramete... Show More
skylink
Motor Control ICs

设置了 TLE9563的 CAN 收发器为 normal模式 但是测试发现,tx和rx引脚没有电平变化,没有正常工作

是否还需要配置其他,或者是否有遗漏的配置?

er_misha
Motor Control ICs
1)There is no option to update iMotion Solution Designer, In the news feed it shows updates for SD package 2) No option for induction motor driver in ... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.