Motor Control ICs Forum Discussions
Hi, I have two questions about the IMC101T-F048 iMOTION™ motor control IC:
1- We designed a system consisting of EVAL-M1-101TF and special power board to control 3-phase PMSM motor.
now I can rotate the motor via MCEdesigner_V2.3 but when i changed the reference speed the motor speed does not change and stays constant at 50 rpm.
I tried to change the maximum and minimum speed limit but I couldn't see any difference.
What could go wrong?
2- We want to integrate the IMC101T-F048 control chip into our design;
a- Is the IMC101T-F048 control chip shipped without software? if so how can i program it and what program or tools are required?
b- Can I change parameter set or speed references via uart (without using MCEDesigner_V2.3 and MCEWizard_V2.3)
Best Regards,
Thanks for respones. You can see all part of circuit diagram below except HV Dc voltage side.
First of all the circuit scheme is for prototype so for this reason , didnt care too much for clean schematic.
At the diagram there is a rectangular that says " didnt soldered" , means that all of those components not soldered and remained open.
If any missunderstood please let me know
Thanks
Show LessHello,
I have a question regarding the nBRAKE signal on the IMD701A.
In the figure 26 of the IMD701A Datasheet the signal is driven by a pullup to high.
In the figure 67 of the IMD701A Datasheet it looks the way that the gate driver can pull this line low.
We would also like to pull the line low from outside in case of emergency.
Now the question is what happens if the XMC1404 Pin is configured as output high by mistake or software bug?
Is the high side driver of the Pin P1.3 deaktivated in this chip? Or may occur damage if P1.3 drives high and the gatedriver or an external device pulls the nBRAKE line low?
Thanks in advance,
Florian
Show LessHello,
i want to implement a few functions using the Script Engine. When I try to compile my code in the MCE Wizard with the script code compile, the error "Can't find script compiler" pops up.
I reinstalled the latest Version of the MCE Wizard, and there is a Compiler folder in the installation package. But the Wizard doesn't find it or its incomplete?
Does someone know what the problem may be?
Best Regards
Show LessI thought RSTN suction is the suction of the socket,But after a certain time,Internal voltage came,After a while and automatically ON,I wonder if someone is broken? There are other ways.
Show Less
Hi!
I notice the driver charge/discharge current DACs in tle92108 are nonlinearly configed (Figure 31/32 in datasheet). Seems like small currents are trimmed with smaller steps, I'm wondering the propose of this. Why do I need to trim the small charging currents with this small presicion (~1mA steps)?
Thanks
BR
Show Less请问一下,使用新版的imotion软件进行软件编程,只能使用这个软件对MCU烧录吗?有没有可以不打开工程的情况下对MCU进行烧录,就像MCEDesiger软件一样。