Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Motor Control ICs Forum Discussions

ElecFun
Motor Control ICs
Hello,   I am getting Source file errors during MCEDesigner installation. Any help here?     Show More
wph1995
Motor Control ICs
Hello everyone; I want to use an IMC302A-F064 to control a three-phase motor rated at 220V @ 1.8A. Is this possible? Regards. Show More
wang1
Motor Control ICs
I used ISD software to debug the voltage control mode, but the motor stopped running after starting. I don't know what the problem is, can you help so... Show More
wang1
Motor Control ICs
Please ask me, I now have two problems when the motor starts.Question 1That is, before I start the motor, I use a tool to fix the rotor of the motor, ... Show More
wang1
Motor Control ICs
I used the isd software to configure 038t storage, but I found that my data could not be stored, and the data was lost after being powered on again. H... Show More
wang1
Motor Control ICs
I use this chip 038T to do infrared remote control, but I can't receive data, may I ask what is going on? Here's what my script says. I used the seria... Show More
n6xb
Motor Control ICs
I am using the EVAL-M7-D111T and EVAL-M7-LVMOS-INV with the single shunt resistor changed to .0025 ohms in Vsp mode. Motor startup is good and motor i... Show More
Translation_Bot
Motor Control ICs
1. In Table 2 of the EVAL-M3- CM615PN evaluation board user manual, the output power is 650 W, and the current per leg is 2.32 arms. How is this curre... Show More
LucasHall
Motor Control ICs
I’m working with a brushless DC motor drive system (IMC101T-T038 iMOTION controller and EVAL-M1-IM828-A MADK inverter board).  The motor is rated at 4... Show More
haines
Motor Control ICs
TLE92108 AMC
solved msg Solved
amc 优势有哪些呢,谢谢   Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.