Announcements

Curious on how you can apply Motor Control ICs to Smart Home Appliances? Register for the ASEAN Smart Home Appliance Webinar here to find out how.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Motor Control ICs Forum Discussions

Motor Control ICs Forum Discussions

Sort by:
cw2611
Motor Control ICs
Hey! I need to calculate the back EMF for my BLDC motor to input to the MCE wizard. I have calculated the value based on your document found here: https://www.infineon.com/dgdl/Infineon-How-to-Measure-Motor-Parameters-ApplicationPresentation-v01_00-EN.pdf?fileId=5546d462566bd0c701568d655bd643ed... Show More
YuTa_4942221
Motor Control ICs
こんにちは、  IPMに関して1つ質問があります。IKCM20L60GDのデータシートP12を確認すると、ダイオードはシャント抵抗の真下に接続されています。このダイオードを実装することは必須ですか?実装しなくても大丈夫ですか? ダイオードの目的はITRIP端子の負バイアスがかからないようにすることだ... Show More
sohail
Motor Control ICs
Hi @Krupashankar               Someone Pl Guide how to Get Variables Data in MCE Designer. As per doc 2.6.5 Variable types and scopeScript engine supp... Show More
cw2611
Motor Control ICs
Hey! I want to run a 36V BLDC motor with peak current at 11A. Do you have any evaluation board that contains both the microcontroller as well as the h... Show More
sohail
Motor Control ICs
Hi,             I write my own  script code in MCE Designer, after compiling it shows the file script Function compile Complete. but this file is not ... Show More
NXTY_hayashi
Motor Control ICs
Hi, I can find nothing on Infineon web site about EVAL-M1-1302. If you have the schematics of EVAL-M1-1302 board, please send me it.   Best Regards, K... Show More
sohail
Motor Control ICs
Hi,        I am using EVAL-M3-302F I want to run simple program Blink led. I tried compile but there is error in IMC300A.h header file & imc300a_port1... Show More
cw2611
Motor Control ICs
Hello  I am trying to configure the BLDC motor using the MCE wizard, can the motor directly be operated using the MCE wizard? or do we need the SPI or... Show More
SBitney
Motor Control ICs
Hi,I'm having issues reaching higher currents when loading down a motor driven by a IMC101. I've got a maximum current limit of 3.5A set, and it will ... Show More
sohail
Motor Control ICs
iMOTION2go
Solved
Hi,           i just got motoin2go board, install MCEDesigner but when i open file IMC101T_V1.02.20_iMOTION2go.irc it give error product mismatch.  i ... Show More
Forum Information

Motor Control ICs

This forum discusses topics on Motor Control ICs - iMOTION™, MOTIX™, MADK etc.