Sep 28, 2021
11:40 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 28, 2021
11:40 PM
The gain drift is the drift of the gain after calibration.
For example, the gain of the current sense amplifier is calibrated at 25 °C with a two point calibration (i.e. using two load currents).
The gain drift is the drift resulting from the device ageing and from the temperature drift (from Tj = -40°C to 150°C).
For example, the gain of the current sense amplifier is calibrated at 25 °C with a two point calibration (i.e. using two load currents).
The gain drift is the drift resulting from the device ageing and from the temperature drift (from Tj = -40°C to 150°C).
- Tags:
- IFX
0 Replies