Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User22801
Level 2
Level 2
10 questions asked 5 questions asked First question asked
The static charge current ICHGST and the static discharge current IDCHGST for static activation are used for two purposes:
1. ICHGST and IDCHGST charge and discharge the gate of the external MOSFETs, which are not controlled in PWM. These MOSFETs can be turned on and turned off faster than the MOSFET controlled in PWM, because the single activation is not relevant for the EMC characterization
2. IDCHGST discharges the gate of the MOSFETs in case of failure

Two criteria must be considered for the configuration of IDCHGST for a short circuit of the MOSFETs:
1. the MOSFETs must be turned off fast enough in order to stay within the safe operating area, considering the possible high drain-source current
2. the MOSFETs may not be turned off too fast, because a high current in combination with stray inductances and a fast turn off can trigger a MOSFET avalanche
That is the reason why IDCHGST is individually configurable for each half-bridge driver, so that these two criteria can be fulfilled for the considered MOSFET type.
0 Likes
0 Replies