Jan 10, 2023
11:12 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 10, 2023
11:12 PM
Hello everybody,
the TLE52062SAKSA1 component has been obsolete for several years, is there a functionally similar alternative? I could also evaluate formats formats (e.g. SMT).
Thanks
1 Reply
Jan 12, 2023
01:52 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 12, 2023
01:52 AM
Hi @dpiazza,
For similar functionality, you can use IFX9201SG. However, some parameters are different from TLE5206-2S like: -
>>Package is PowerSO-12.
>>Min and max current are 6A and 8A respectively.
>>Operating voltage 4.5v-36v.
>>Also, output control is different( PWM/DIR).
>> It can support a max 11khz PWM and additionally support open load diagnosis.
Note:- It is not the exact replacement for the TLE5206-2S. so for your application please refer to the datasheet of the IFX9201SG.
Best Regards
Sahil Kumar